Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed - how to boot from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 364 subscribers
  • Views 5071 views
  • Users 0 members are here
Related

MicroZed - how to boot from SD card

e14 Contributor
e14 Contributor over 12 years ago

Hi,
i have done a lot of reading regarding the MicroZed SD card boot but still cannot manage.

All of the information seems to be for the ZedBoard. Where could i find a boot.bin file for the MicroZed?

As i understand the boot.bin will contain the u-boot, fsbl and PL bitstream.

The getting started states the following:
Download and unzip the MicroZed_Linux_sd_image archive from www.microzed.org.

This image, however will not boot. Nothing will appear in the console.

Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hi,
    thanks for the reply. I have the 7010 MicroZed. The board will boot when i boot from the QSPI image that came preinstalled with the kit. I see the log and can use the BusyBox interface. Therefore i assume that the USB-UART & putty are properly installed.

    When i set the jumpers JP3 to JP1 to boot from SD card then i don't get anything in the log. Also, the blue D2 LED will not light up.
    Only green D5 and red D3 light up.

    How could i furter debug the configure phase?

    Regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ldeevans
    0 ldeevans over 12 years ago in reply to e14 Contributor

    The 4GB SDcard supplied is formatted as a FAT16 drive which (my) Win7 doesn't seem to recognise. Use a Linux distro/machine and reformat it as a FAT32 partition, eg. use "mkfs.vfat /dev/sdd1", where sdd1 is your appropriate target as shown by "sfdisk -l" (on my Linux distro the partition type id came up as win95).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ldeevans
    0 ldeevans over 11 years ago in reply to ldeevans

    And you will need to use "fdisk /dev/sdd" and enable (toggle?) the boot flag for the primary partition, to allow zedboard to boot.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ldeevans
    0 ldeevans over 11 years ago in reply to ldeevans

    And you will need to use "fdisk /dev/sdd" and enable (toggle?) the boot flag for the primary partition, to allow zedboard to boot.