Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed - how to boot from SD card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 16 replies
  • Subscribers 364 subscribers
  • Views 5071 views
  • Users 0 members are here
Related

MicroZed - how to boot from SD card

e14 Contributor
e14 Contributor over 12 years ago

Hi,
i have done a lot of reading regarding the MicroZed SD card boot but still cannot manage.

All of the information seems to be for the ZedBoard. Where could i find a boot.bin file for the MicroZed?

As i understand the boot.bin will contain the u-boot, fsbl and PL bitstream.

The getting started states the following:
Download and unzip the MicroZed_Linux_sd_image archive from www.microzed.org.

This image, however will not boot. Nothing will appear in the console.

Regards

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I have a newer 7010 MicroZed board. If I put the Linux boot.bin and associated files on mentioned in this thread, I can boot Linux just fine from the SD card. I have a fairly simple configuration that boots from the QSPI flash if I program the *.mcs file in and set the jumpers, but if I copy the BOOT.bin file onto the micro SD card, I don't get the blue programmed light, and I can't communicate via the UART. I'm using Xilinx SDK 2015.3 to create both the .mcs and BOOT.bin files. Any ideas as to why this doesn't work?

    Thanks, Jerry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    I have a newer 7010 MicroZed board. If I put the Linux boot.bin and associated files on mentioned in this thread, I can boot Linux just fine from the SD card. I have a fairly simple configuration that boots from the QSPI flash if I program the *.mcs file in and set the jumpers, but if I copy the BOOT.bin file onto the micro SD card, I don't get the blue programmed light, and I can't communicate via the UART. I'm using Xilinx SDK 2015.3 to create both the .mcs and BOOT.bin files. Any ideas as to why this doesn't work?

    Thanks, Jerry