Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design 1V Power Rail Question
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 927 views
  • Users 0 members are here
Related

1V Power Rail Question

e14 Contributor
e14 Contributor over 11 years ago

I was looking at the 1.0V power section on the microzed (U17 and surrounding parts).

When the microzeds are in the Breakout Carrier and powered up, I am only seeing 0.2 Volts across C57. This is true for all my microzeds.

Shouldn't this supply be 1 Volt?

Cheers,
David

-EDIT-
1 of my 4 microzeds does in fact show 1.0V for this node.

Any ideas why the others do not?

  • Sign in to reply
  • Cancel
Parents
  • ctammann
    0 ctammann over 11 years ago

    Hi David.  Do you also see 0.2V if you do NOT have it plugged into the breakout carrier?  Is there a bit stream loaded in the FPGA?

    Do you have an oscilloscope you could put on the 1V during startup to see if it is coming up and turning off or if it isn't coming up at all?

    I haven't seen this before.  It could be a result of the input supply having insufficient power.  If the input supply is limiting, it could cause various rails to not start.  Are there any heavy loads on the carrier?  Are you trying to power it off a USB port?  If so, try powering it off a DC source or off say a USB cell phone charger.

    Thanks

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ctammann
    0 ctammann over 11 years ago

    Hi David.  Do you also see 0.2V if you do NOT have it plugged into the breakout carrier?  Is there a bit stream loaded in the FPGA?

    Do you have an oscilloscope you could put on the 1V during startup to see if it is coming up and turning off or if it isn't coming up at all?

    I haven't seen this before.  It could be a result of the input supply having insufficient power.  If the input supply is limiting, it could cause various rails to not start.  Are there any heavy loads on the carrier?  Are you trying to power it off a USB port?  If so, try powering it off a DC source or off say a USB cell phone charger.

    Thanks

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to ctammann

    Hi Chris,
    Good ideas.

    I've been running off an AC adapter rated at 2 Amps, not a USB port. I swapped it out for another 2A rated adapter and still see the same behavior.

    I removed the uZed from the carrier and powered it from the AC adapter. Now, none of the regulators are producing outputs, rather than half of them (see my other post). This is what I would expect, since they are enabled in series.

    I monitored the 1V power bus with a scope. Upon applying power, the voltage increases from 0V to 0.2V in about 200 microseconds and stays steady at 0.2V.

    Cheers,
    David