Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design 1V Power Rail Question
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 927 views
  • Users 0 members are here
Related

1V Power Rail Question

e14 Contributor
e14 Contributor over 11 years ago

I was looking at the 1.0V power section on the microzed (U17 and surrounding parts).

When the microzeds are in the Breakout Carrier and powered up, I am only seeing 0.2 Volts across C57. This is true for all my microzeds.

Shouldn't this supply be 1 Volt?

Cheers,
David

-EDIT-
1 of my 4 microzeds does in fact show 1.0V for this node.

Any ideas why the others do not?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I measured the voltages at the output of each regulator for 4 uZeds. I tried to make a table, but I can't seem to format these messages.

    I'll summarize by saying that 1 uZed appeared healthy with the 1.0V supply measured as 1.0V. The 1.5V supply measured 1.49. The 1.8V supply measured 1.80V. The 3.3V supply measured 3.28V. This is with Vin=4.2V.

    3 other uZeds were virtually identical with: 1.0V supply measured 0.2V. 1.5V supply measured 1.5V. 1.8V supply measured 0.14V. 3.3V supply measured 3.28V. All with Vin=4.1V.

    So, in summary I have 1 good uZed and 3 uZeds that only have half the supplies operating properly.

    Any suggestions on what might be the root cause?

    Cheers,
    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    So I removed the 1V power supply section on the microzed and drove it from an external, metered supply so that I could get an idea of how much current the board would draw.

    This did not shed much light on the problem. The board would gladly sink 3 Amps (applied for a couple hundred milliseconds). So I pulled the PHY chip (it's on the 1V supply bus) and still no joy.

    So the only chip left was of course the Zynq itself. I pulled it and the 1V bus is now happy. I don't see how this helps me much. What can I do but say that, out of the box, the Zynq chips draw large currents on the 1V bus?

    This really shakes my confidence in just about every aspect of my project.

    I did notice that all my microzeds have a bunch of re-work. You can tell from the solder flux residue at several places on the board.

    Why would brand new microzeds have a bunch of re-work? I'll post this as a separate thread.

    David

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    So I removed the 1V power supply section on the microzed and drove it from an external, metered supply so that I could get an idea of how much current the board would draw.

    This did not shed much light on the problem. The board would gladly sink 3 Amps (applied for a couple hundred milliseconds). So I pulled the PHY chip (it's on the 1V supply bus) and still no joy.

    So the only chip left was of course the Zynq itself. I pulled it and the 1V bus is now happy. I don't see how this helps me much. What can I do but say that, out of the box, the Zynq chips draw large currents on the 1V bus?

    This really shakes my confidence in just about every aspect of my project.

    I did notice that all my microzeds have a bunch of re-work. You can tell from the solder flux residue at several places on the board.

    Why would brand new microzeds have a bunch of re-work? I'll post this as a separate thread.

    David