Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed Power Supply Enable Issue
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 361 subscribers
  • Views 757 views
  • Users 0 members are here
Related

Microzed Power Supply Enable Issue

e14 Contributor
e14 Contributor over 12 years ago

Hello,


I wanted to report an issue that I've encountered with the Microzed board, in hopes that it can be improved in future revisions or that it can save others some time. I believe this is a bug in the hardware design, but please let me know if I've misunderstood something. I'm using Rev F of the board.


The 1.8V switcher is enabled by the power good (PG) output of the 1.0V switcher. The PG pin is open-collector, so it must be pulled up. This is done by R42, which pulls up to 1.0V, with R88 as a pull down making a voltage divider. The nominal value of PG_1V_10 when high is 1V*5k/(1k+5k) = 830mV.


This net drives the EN pin of U15. The datasheet for TLV62130RGT (http://www.ti.com/lit/ds/symlink/tlv62130.pdf) states that the minimum "high" input voltage for this pin is 0.9V, so the microzed is not meeting it. It works most of the time, but while debugging some intermittent problems with a USB device, we found that the 1.8V switcher was occasionally kicking off and collapsing for a short period of time (but long enough to cause problems communicating with the USB phy). We definitely had one board that had more problems than others, so there is also some board-to-board variance.


We've worked around this problem by blue-wiring the pullup to our 5V input voltage. I would suggest that microzed designers do the same in future revisions, perhaps with a zener to prevent the net from rising above the 7V max allowable voltage in the case where a higher input voltage is used to power the board.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Jeff,

     

    Thanks for the observation, we are always working to make our products better. Our engineers followed up on your input and we will be changing the MicroZed Bill of Materials to reduce the value of R42 to 240 ohms which, as you pointed out, will increase the nominal value of PG_1V_10.

     

    Each MicroZed has been functionally tested prior to shipment and we have not observed any failures, even in the units we tested for the extended temperature range, so we don't anticipate anyone having issue with the current boards.

     

    If anyone does experience problems please contact me directly.

     

    Regards,

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Jeff,

     

    Thanks for the observation, we are always working to make our products better. Our engineers followed up on your input and we will be changing the MicroZed Bill of Materials to reduce the value of R42 to 240 ohms which, as you pointed out, will increase the nominal value of PG_1V_10.

     

    Each MicroZed has been functionally tested prior to shipment and we have not observed any failures, even in the units we tested for the extended temperature range, so we don't anticipate anyone having issue with the current boards.

     

    If anyone does experience problems please contact me directly.

     

    Regards,

     

    -Gary