Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Peripheral_Tester lab fails on 2014.2 Xilinx SDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 363 subscribers
  • Views 782 views
  • Users 0 members are here
Related

Peripheral_Tester lab fails on 2014.2 Xilinx SDK

ghalady
ghalady over 12 years ago

The Microzed's tutorial lab3 to run Peripherals_test fails with the following error:

18:38:40 **** Build of configuration Debug for project Peripheral_Tester ****
make all
'Building file: ../src/testperiph.c'
'Invoking: ARM gcc compiler'
arm-xilinx-eabi-gcc -Wall -O0 -g3 -c -fmessage-length=0 -I../../standalone_bsp_0/ps7_cortexa9_0/include -MMD -MP -MF"src/testperiph.d" -MT"src/testperiph.d" -o "src/testperiph.o" "../src/testperiph.c"
../src/testperiph.c:44:21: fatal error: xemacps.h: No such file or directory
#include "xemacps.h"
                     ^
compilation terminated.
make: *** [src/testperiph.o] Error 1

18:38:41 Build Finished (took 1s.380ms)

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    It looks like your application code is looking for a peripheral (the PS Ethernet MAC) that is not included in the selected BSP. Make sure you are referencing the correct BSP for the application. If that is correct you might try a 'Clean' operation under  'Project' on the SDK toolbar to make sure everything is built to the latest exported hardware and then rebuild all if that is not done automatically.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I ran into the same problem when following the Speedway lab 3 - to solve this, select the system.mss file under your bsp folder in the SDK, press 're-generate BSP sources'

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ghalady
    0 ghalady over 12 years ago

    Thanks Ronny,
    I could get this work with the re-generation of BSP. However, I have issues with getting the dmatest to work on Microzed right now. Have posted this as a separate topic. Hoping to hear back from someone.

    Regards
    Girish Halady

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • nick0559
    0 nick0559 over 11 years ago

    I tried the BSP regeneration and still the error was there.

    I then made new BSP and included Lwip support.  I changed the referenced BSP to this new one and everything worked fine.

    Nick