Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design QSPI Flash Chip Select Drive Strength
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 1007 views
  • Users 0 members are here
Related

QSPI Flash Chip Select Drive Strength

e14 Contributor
e14 Contributor over 11 years ago

Hi,

Just found out there is a 240 ohm pull-up resistor on the QSPI_1_CS# (QSPI flash chip select) in MicroZed schematic and the PS_MIO1 needs to sink >13mA to drive the QSPI_1_CS# to 0V.  But PS MIO is rated 8mA in the datasheet.  Is there a special reason to pull-up the QSPI_1_CS# with a 240 ohm?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    We measured R71’s low signal level with the following resistors:

     

    1.   R71 at 240 yields an output low(max) of 200mV.
    2.   R71 at 100K yields an output low (max) of 60mV.

     

    These values were captured using a DMM. By inference, we can get I by: (3.3V-0.2V)/R71 = 3.1V/240 = 12.9mA.  At 100K we see 32.4uA.

     

    We are planning to increase R71 for our next MicroZed build. Thanks for bringing this to our attention.

     

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 11 years ago

    We measured R71’s low signal level with the following resistors:

     

    1.   R71 at 240 yields an output low(max) of 200mV.
    2.   R71 at 100K yields an output low (max) of 60mV.

     

    These values were captured using a DMM. By inference, we can get I by: (3.3V-0.2V)/R71 = 3.1V/240 = 12.9mA.  At 100K we see 32.4uA.

     

    We are planning to increase R71 for our next MicroZed build. Thanks for bringing this to our attention.

     

    Bryan