Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MicroZed: driving LEDs using the user MIOs of PMOD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 361 subscribers
  • Views 939 views
  • Users 0 members are here
Related

MicroZed: driving LEDs using the user MIOs of PMOD

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I want to use the user MIO that are connected to the PMOD on the MicroZed board to drive the LEDs (via transistor switch) and the MOSFET driver in my PoC design. I have several questions related to both HW and SW that I would be very grateful if someone can help:
1. What is the maximum current these MIO pins can deliver?
2. How could I control them in my SW applications? Is that possible to include these MIO pins in the file system of the Linux OS?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Per the Zynq data sheet ds187( http://www.xilinx.com/support/documentation/data_sheets/ds187-XC7Z010-XC7Z020-Data-Sheet.pdf  ) the MIO pins can drive 8 mA. As these signals are directly connected to the Zynq device you should take care not to damage the device with electrostatic discharge or out of range voltages.

     

    The easiest way to control the MIO under Linux is probable SysFs functions. Here are a couple of forum posts related to using SysFs:

     

    http://zedboard.org/content/which-tutorial-linux-pl-access

    http://zedboard.org/content/blink-led-linaroubuntu1110

    http://zedboard.org/content/writing-gpio-linux-application-microzed

     

    If you would prefer to write a C application under Linux and control the MIO that way there is an example in the ZedBoard Concept Tools and Techniques (CTT) tutorial that might be helpful: http://zedboard.org/support/design/1521/11

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Gary,

    Just a quick update, as promised. Based on the information you provided, I decided to use the sysfs API and managed to be successfully flashing our LEDs with these MIO exported on the PMOD connector. Thanks for your help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hi Gary,

    Just a quick update, as promised. Based on the information you provided, I decided to use the sysfs API and managed to be successfully flashing our LEDs with these MIO exported on the PMOD connector. Thanks for your help.