Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design FFT demo
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 828 views
  • Users 0 members are here
Related

FFT demo

suppamax
suppamax over 11 years ago

Hi,

I am trying to duplicate the project described here
http://www.wiki.xilinx.com/Zynq-7000+AP+SoC+Spectrum+Analyzer+part+5+-+Accelerating+Software+-+Accelerating+an+FFT+with+ACP+Coprocessor+Tech+Tip+2014.3
on microzed.

I simplified it by removing all HDMI-related ports, which are not interesting for me.

In SDK, I created a simple helloword SW, just to verify that the basic features are working, but the zynq wouldn't boot.

During synthesis I receive this warning message

WARNING: [Synth 8-4446] all outputs are unconnected for this instance and logic may be removed [/home/suppamax/Designs/AXI_FFT/hw/pl_trd_fft_only/project/zynq_base_trd_2014.4.srcs/sources_1/bd/system_top/hdl/system_top_wrapper.v:78]

but in the end the placing report shows ~30% of the slices used
+----------------------------+-------+-------+-----------+-------+
|          Site Type         |  Used | Fixed | Available | Util% |
+----------------------------+-------+-------+-----------+-------+
| Slice LUTs                 | 19960 |     0 |     53200 | 37.51 |
|   LUT as Logic             | 17425 |     0 |     53200 | 32.75 |
|   LUT as Memory            |  2535 |     0 |     17400 | 14.56 |
|     LUT as Distributed RAM |   914 |     0 |           |       |
|     LUT as Shift Register  |  1621 |     0 |           |       |
| Slice Registers            | 29154 |     0 |    106400 | 27.40 |
|   Register as Flip Flop    | 29154 |     0 |    106400 | 27.40 |
|   Register as Latch        |     0 |     0 |    106400 |  0.00 |
| F7 Muxes                   |    92 |     0 |     26600 |  0.34 |
| F8 Muxes                   |     0 |     0 |     13300 |  0.00 |
+----------------------------+-------+-------+-----------+-------+

Could you suggest how to debug further?

I copy below the tcl script to regenerate the project.

---


################################################################
# This is a generated script based on design: system_top
#
# Though there are limitations about the generated script,
# the main purpose of this utility is to make learning
# IP Integrator Tcl commands easier.
################################################################

################################################################
# Check if script is running in correct Vivado version.
################################################################
set scripts_vivado_version 2014.4
set current_vivado_version [version -short]

if { [string first $scripts_vivado_version $current_vivado_version] == -1 } {
   puts ""
   puts "ERROR: This script was generated using Vivado <$scripts_vivado_version> and is being run in <$current_vivado_version> of Vivado. Please run the script in Vivado <$scripts_vivado_version> then open the design in Vivado <$current_vivado_version>. Upgrade the design by running "Tools => Report => Report IP Status...", then run write_bd_tcl to create an updated script."

   return 1
}

################################################################
# START
################################################################

# To test this script, run the following commands from Vivado Tcl console:
# source system_top_script.tcl

# If you do not already have a project created,
# you can create a project using the following command:
#    create_project project_1 myproj -part xc7z020clg400-1
#    set_property BOARD_PART em.avnet.com:microzed_7020:part0:1.0 [current_project]


# CHANGE DESIGN NAME HERE
set design_name system_top

# If you do not already have an existing IP Integrator design open,
# you can create a design using the following command:
#    create_bd_design $design_name

# CHECKING IF PROJECT EXISTS
if { [get_projects -quiet] eq "" } {
   puts "ERROR: Please open or create a project!"
   return 1
}


# Creating design if needed
set errMsg ""
set nRet 0

set cur_design [current_bd_design -quiet]
set list_cells [get_bd_cells -quiet]

if { ${design_name} eq "" } {
   # USE CASES:
   #    1) Design_name not set

   set errMsg "ERROR: Please set the variable <design_name> to a non-empty value."
   set nRet 1

} elseif { ${cur_design} ne "" && ${list_cells} eq "" } {
   # USE CASES:
   #    2): Current design opened AND is empty AND names same.
   #    3): Current design opened AND is empty AND names diff; design_name NOT in project.
   #    4): Current design opened AND is empty AND names diff; design_name exists in project.

   if { $cur_design ne $design_name } {
      puts "INFO: Changing value of <design_name> from <$design_name> to <$cur_design> since current design is empty."
      set design_name [get_property NAME $cur_design]
   }
   puts "INFO: Constructing design in IPI design <$cur_design>..."

} elseif { ${cur_design} ne "" && $list_cells ne "" && $cur_design eq $design_name } {
   # USE CASES:
   #    5) Current design opened AND has components AND same names.

   set errMsg "ERROR: Design <$design_name> already exists in your project, please set the variable <design_name> to another value."
   set nRet 1
} elseif { [get_files -quiet ${design_name}.bd] ne "" } {
   # USE CASES:
   #    6) Current opened design, has components, but diff names, design_name exists in project.
   #    7) No opened design, design_name exists in project.

   set errMsg "ERROR: Design <$design_name> already exists in your project, please set the variable <design_name> to another value."
   set nRet 2

} else {
   # USE CASES:
   #    8) No opened design, design_name not in project.
   #    9) Current opened design, has components, but diff names, design_name not in project.

   puts "INFO: Currently there is no design <$design_name> in project, so creating one..."

   create_bd_design $design_name

   puts "INFO: Making design <$design_name> as current_bd_design."
   current_bd_design $design_name

}

puts "INFO: Currently the variable <design_name> is equal to "$design_name"."

if { $nRet != 0 } {
   puts $errMsg
   return $nRet
}

##################################################################
# DESIGN PROCs
##################################################################


# Hierarchical cell: memory
proc create_hier_cell_memory { parentCell nameHier } {

  if { $parentCell eq "" || $nameHier eq "" } {
     puts "ERROR: create_hier_cell_memory() - Empty argument(s)!"
     return
  }

  # Get object for parentCell
  set parentObj [get_bd_cells $parentCell]
  if { $parentObj == "" } {
     puts "ERROR: Unable to find parent cell <$parentCell>!"
     return
  }

  # Make sure parentObj is hier blk
  set parentType [get_property TYPE $parentObj]
  if { $parentType ne "hier" } {
     puts "ERROR: Parent <$parentObj> has TYPE = <$parentType>. Expected to be <hier>."
     return
  }

  # Save current instance; Restore later
  set oldCurInst [current_bd_instance .]

  # Set parent object as current
  current_bd_instance $parentObj

  # Create cell and set as current instance
  set hier_obj [create_bd_cell -type hier $nameHier]
  current_bd_instance $hier_obj

  # Create interface pins
  create_bd_intf_pin -mode Master -vlnv xilinx.com:interface:aximm_rtl:1.0 M00_AXI
  create_bd_intf_pin -mode Master -vlnv xilinx.com:interface:aximm_rtl:1.0 M00_AXI1
  create_bd_intf_pin -mode Master -vlnv xilinx.com:interface:axis_rtl:1.0 M_AXIS_MM2S
  create_bd_intf_pin -mode Slave -vlnv xilinx.com:interface:aximm_rtl:1.0 S01_AXI
  create_bd_intf_pin -mode Slave -vlnv xilinx.com:interface:aximm_rtl:1.0 S_AXI
  create_bd_intf_pin -mode Slave -vlnv xilinx.com:interface:axis_rtl:1.0 S_AXIS_S2MM
  create_bd_intf_pin -mode Slave -vlnv xilinx.com:interface:axis_rtl:1.0 S_AXIS_S2MM1
  create_bd_intf_pin -mode Slave -vlnv xilinx.com:interface:aximm_rtl:1.0 S_AXI_LITE
  create_bd_intf_pin -mode Slave -vlnv xilinx.com:interface:aximm_rtl:1.0 S_AXI_LITE1

  # Create pins
  create_bd_pin -dir O -type intr PerfMon_intr
  create_bd_pin -dir I -type clk core_aclk
  create_bd_pin -dir I -from 0 -to 0 -type rst core_aresetn
  create_bd_pin -dir O -type intr mm2s_introut
  create_bd_pin -dir O -type intr s2mm_introut
  create_bd_pin -dir O -type intr s2mm_introut1
  create_bd_pin -dir I -type clk s_axi_aclk

  # Create instance: axi_interconnect_hp0, and set properties
  set axi_interconnect_hp0 [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_interconnect:2.1 axi_interconnect_hp0 ]
  set_property -dict [ list CONFIG.ENABLE_ADVANCED_OPTIONS {1} CONFIG.M00_HAS_DATA_FIFO {2} CONFIG.M00_HAS_REGSLICE {1} CONFIG.NUM_MI {1} CONFIG.NUM_SI {2} CONFIG.S00_HAS_REGSLICE {1} CONFIG.S01_HAS_REGSLICE {1} CONFIG.STRATEGY {2}  ] $axi_interconnect_hp0

  # Create instance: axi_interconnect_hp2, and set properties
  set axi_interconnect_hp2 [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_interconnect:2.1 axi_interconnect_hp2 ]
  set_property -dict [ list CONFIG.ENABLE_ADVANCED_OPTIONS {1} CONFIG.ENABLE_PROTOCOL_CHECKERS {0} CONFIG.M00_HAS_DATA_FIFO {2} CONFIG.M00_HAS_REGSLICE {1} CONFIG.NUM_MI {1} CONFIG.NUM_SI {2} CONFIG.S00_HAS_REGSLICE {1} CONFIG.S01_HAS_REGSLICE {1} CONFIG.STRATEGY {2} CONFIG.XBAR_DATA_WIDTH {64}  ] $axi_interconnect_hp2

  # Create instance: axi_perf_mon_1, and set properties
  set axi_perf_mon_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_perf_mon:5.0 axi_perf_mon_1 ]
  set_property -dict [ list CONFIG.C_NUM_MONITOR_SLOTS {2} CONFIG.C_NUM_OF_COUNTERS {4} CONFIG.C_SLOT_0_AXI_PROTOCOL {AXI3} CONFIG.C_SLOT_1_AXI_PROTOCOL {AXI3}  ] $axi_perf_mon_1

  # Create instance: axi_vdma_1, and set properties
  set axi_vdma_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_vdma:6.2 axi_vdma_1 ]
  set_property -dict [ list CONFIG.c_enable_debug_info_11 {1} CONFIG.c_enable_debug_info_15 {1} CONFIG.c_include_mm2s {0} CONFIG.c_include_s2mm_dre {0} CONFIG.c_include_s2mm_sf {0} CONFIG.c_num_fstores {1} CONFIG.c_s2mm_genlock_mode {2} CONFIG.c_s2mm_linebuffer_depth {4096} CONFIG.c_s2mm_max_burst_length {16} CONFIG.c_s2mm_sof_enable {1}  ] $axi_vdma_1

  # Create instance: axi_vdma_2, and set properties
  set axi_vdma_2 [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_vdma:6.2 axi_vdma_2 ]
  set_property -dict [ list CONFIG.c_enable_debug_info_7 {1} CONFIG.c_enable_debug_info_15 {1} CONFIG.c_m_axi_mm2s_data_width {32} CONFIG.c_m_axis_mm2s_tdata_width {16} CONFIG.c_mm2s_genlock_mode {3} CONFIG.c_mm2s_linebuffer_depth {4096} CONFIG.c_mm2s_max_burst_length {16} CONFIG.c_num_fstores {1} CONFIG.c_s2mm_genlock_mode {2} CONFIG.c_s2mm_linebuffer_depth {4096} CONFIG.c_s2mm_max_burst_length {16} CONFIG.c_use_mm2s_fsync {1} CONFIG.c_use_s2mm_fsync {2}  ] $axi_vdma_2

  # Create interface connections
  connect_bd_intf_net -intf_net FILTER_VDMA_M_AXIS_MM2S [get_bd_intf_pins M_AXIS_MM2S] [get_bd_intf_pins axi_vdma_2/M_AXIS_MM2S]
  connect_bd_intf_net -intf_net S00_AXI_2 [get_bd_intf_pins axi_interconnect_hp2/S00_AXI] [get_bd_intf_pins axi_vdma_2/M_AXI_MM2S]
  connect_bd_intf_net -intf_net S00_AXI_3 [get_bd_intf_pins axi_interconnect_hp0/S00_AXI] [get_bd_intf_pins axi_vdma_1/M_AXI_S2MM]
  connect_bd_intf_net -intf_net S01_AXI_2 [get_bd_intf_pins axi_interconnect_hp2/S01_AXI] [get_bd_intf_pins axi_vdma_2/M_AXI_S2MM]
  connect_bd_intf_net -intf_net Video_Processing_OUTPUT_STREAM [get_bd_intf_pins S_AXIS_S2MM] [get_bd_intf_pins axi_vdma_2/S_AXIS_S2MM]
  connect_bd_intf_net -intf_net axi4_gp0_M03_AXI [get_bd_intf_pins S_AXI] [get_bd_intf_pins axi_perf_mon_1/S_AXI]
  connect_bd_intf_net -intf_net axi_interconnect_1_m00_axi [get_bd_intf_pins M00_AXI] [get_bd_intf_pins axi_interconnect_hp0/M00_AXI]
  connect_bd_intf_net -intf_net axi_interconnect_1_m00_axi [get_bd_intf_pins M00_AXI] [get_bd_intf_pins axi_perf_mon_1/SLOT_0_AXI]
  connect_bd_intf_net -intf_net axi_interconnect_3_m00_axi [get_bd_intf_pins M00_AXI1] [get_bd_intf_pins axi_interconnect_hp2/M00_AXI]
  connect_bd_intf_net -intf_net axi_interconnect_3_m00_axi [get_bd_intf_pins M00_AXI1] [get_bd_intf_pins axi_perf_mon_1/SLOT_1_AXI]
  connect_bd_intf_net -intf_net axi_interconnect_gp0_M01_AXI [get_bd_intf_pins S_AXI_LITE1] [get_bd_intf_pins axi_vdma_1/S_AXI_LITE]
  connect_bd_intf_net -intf_net axi_interconnect_gp0_M02_AXI [get_bd_intf_pins S_AXI_LITE] [get_bd_intf_pins axi_vdma_2/S_AXI_LITE]
  connect_bd_intf_net -intf_net fmc_hdmi_input_video_out [get_bd_intf_pins S_AXIS_S2MM1] [get_bd_intf_pins axi_vdma_1/S_AXIS_S2MM]
  connect_bd_intf_net -intf_net s01_axi_1 [get_bd_intf_pins S01_AXI] [get_bd_intf_pins axi_interconnect_hp0/S01_AXI]

  # Create port connections
  connect_bd_net -net axi_perf_mon_1_interrupt [get_bd_pins PerfMon_intr] [get_bd_pins axi_perf_mon_1/interrupt]
  connect_bd_net -net axi_vdma_1_s2mm_fsync_out [get_bd_pins axi_vdma_1/s2mm_fsync_out] [get_bd_pins axi_vdma_2/mm2s_fsync]
  connect_bd_net -net clk_150mhz [get_bd_pins core_aclk] [get_bd_pins axi_interconnect_hp0/ACLK] [get_bd_pins axi_interconnect_hp0/M00_ACLK] [get_bd_pins axi_interconnect_hp0/S00_ACLK] [get_bd_pins axi_interconnect_hp0/S01_ACLK] [get_bd_pins axi_interconnect_hp2/ACLK] [get_bd_pins axi_interconnect_hp2/M00_ACLK] [get_bd_pins axi_interconnect_hp2/S00_ACLK] [get_bd_pins axi_interconnect_hp2/S01_ACLK] [get_bd_pins axi_perf_mon_1/core_aclk] [get_bd_pins axi_perf_mon_1/slot_0_axi_aclk] [get_bd_pins axi_perf_mon_1/slot_1_axi_aclk] [get_bd_pins axi_vdma_1/m_axi_s2mm_aclk] [get_bd_pins axi_vdma_1/s_axis_s2mm_aclk] [get_bd_pins axi_vdma_2/m_axi_mm2s_aclk] [get_bd_pins axi_vdma_2/m_axi_s2mm_aclk] [get_bd_pins axi_vdma_2/m_axis_mm2s_aclk] [get_bd_pins axi_vdma_2/s_axis_s2mm_aclk]
  connect_bd_net -net clk_75mhz [get_bd_pins s_axi_aclk] [get_bd_pins axi_perf_mon_1/s_axi_aclk] [get_bd_pins axi_vdma_1/s_axi_lite_aclk] [get_bd_pins axi_vdma_2/s_axi_lite_aclk]
  connect_bd_net -net filter_vdma_mm2s_int_1 [get_bd_pins mm2s_introut] [get_bd_pins axi_vdma_2/mm2s_introut]
  connect_bd_net -net filter_vdma_s2mm_int_1 [get_bd_pins s2mm_introut] [get_bd_pins axi_vdma_2/s2mm_introut]
  connect_bd_net -net proc_sys_reset_1_interconnect_aresetn [get_bd_pins core_aresetn] [get_bd_pins axi_interconnect_hp0/ARESETN] [get_bd_pins axi_interconnect_hp0/M00_ARESETN] [get_bd_pins axi_interconnect_hp0/S00_ARESETN] [get_bd_pins axi_interconnect_hp0/S01_ARESETN] [get_bd_pins axi_interconnect_hp2/ARESETN] [get_bd_pins axi_interconnect_hp2/M00_ARESETN] [get_bd_pins axi_interconnect_hp2/S00_ARESETN] [get_bd_pins axi_interconnect_hp2/S01_ARESETN] [get_bd_pins axi_perf_mon_1/core_aresetn] [get_bd_pins axi_perf_mon_1/s_axi_aresetn] [get_bd_pins axi_perf_mon_1/slot_0_axi_aresetn] [get_bd_pins axi_perf_mon_1/slot_1_axi_aresetn] [get_bd_pins axi_vdma_1/axi_resetn] [get_bd_pins axi_vdma_2/axi_resetn]
  connect_bd_net -net tpg_vdma_s2mm_int_1 [get_bd_pins s2mm_introut1] [get_bd_pins axi_vdma_1/s2mm_introut]
 
  # Restore current instance
  current_bd_instance $oldCurInst
}

# Hierarchical cell: FFT
proc create_hier_cell_FFT { parentCell nameHier } {

  if { $parentCell eq "" || $nameHier eq "" } {
     puts "ERROR: create_hier_cell_FFT() - Empty argument(s)!"
     return
  }

  # Get object for parentCell
  set parentObj [get_bd_cells $parentCell]
  if { $parentObj == "" } {
     puts "ERROR: Unable to find parent cell <$parentCell>!"
     return
  }

  # Make sure parentObj is hier blk
  set parentType [get_property TYPE $parentObj]
  if { $parentType ne "hier" } {
     puts "ERROR: Parent <$parentObj> has TYPE = <$parentType>. Expected to be <hier>."
     return
  }

  # Save current instance; Restore later
  set oldCurInst [current_bd_instance .]

  # Set parent object as current
  current_bd_instance $parentObj

  # Create cell and set as current instance
  set hier_obj [create_bd_cell -type hier $nameHier]
  current_bd_instance $hier_obj

  # Create interface pins
  create_bd_intf_pin -mode Master -vlnv xilinx.com:interface:aximm_rtl:1.0 M_AXI_MM
  create_bd_intf_pin -mode Slave -vlnv xilinx.com:interface:aximm_rtl:1.0 S_AXI_CTRL

  # Create pins
  create_bd_pin -dir I -from 0 -to 0 ARESETN
  create_bd_pin -dir I -type clk M_AXI_CLK
  create_bd_pin -dir I S02_ACLK
  create_bd_pin -dir I -from 0 -to 0 S02_ARESETN
  create_bd_pin -dir I -type clk S_AXI_CLK
  create_bd_pin -dir O -type intr mm2s_introut
  create_bd_pin -dir O -type intr s2mm_introut

  # Create instance: FFT, and set properties
  set FFT [ create_bd_cell -type ip -vlnv xilinx.com:ip:xfft:9.0 FFT ]
  set_property -dict [ list CONFIG.aresetn {true} CONFIG.complex_mult_type {use_mults_performance} CONFIG.data_format {floating_point} CONFIG.implementation_options {pipelined_streaming_io} CONFIG.output_ordering {natural_order} CONFIG.transform_length {4096}  ] $FFT

  # Create instance: axi_dma, and set properties
  set axi_dma [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_dma:7.1 axi_dma ]
  set_property -dict [ list CONFIG.c_include_sg {0} CONFIG.c_m_axi_mm2s_data_width {64} CONFIG.c_m_axi_s2mm_data_width {64} CONFIG.c_m_axis_mm2s_tdata_width {64} CONFIG.c_mm2s_burst_size {16} CONFIG.c_s2mm_burst_size {16} CONFIG.c_sg_length_width {17}  ] $axi_dma

  # Create instance: axi_interconnect, and set properties
  set axi_interconnect [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_interconnect:2.1 axi_interconnect ]
  set_property -dict [ list CONFIG.ENABLE_ADVANCED_OPTIONS {1} CONFIG.M00_HAS_REGSLICE {1} CONFIG.NUM_MI {1} CONFIG.NUM_SI {2} CONFIG.S00_HAS_REGSLICE {1} CONFIG.S01_HAS_REGSLICE {1} CONFIG.S02_HAS_REGSLICE {1} CONFIG.XBAR_DATA_WIDTH {64}  ] $axi_interconnect

  # Create instance: xlconstant_1, and set properties
  set xlconstant_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:xlconstant:1.1 xlconstant_1 ]
  set_property -dict [ list CONFIG.CONST_VAL {0}  ] $xlconstant_1

  # Create instance: xlconstant_2, and set properties
  set xlconstant_2 [ create_bd_cell -type ip -vlnv xilinx.com:ip:xlconstant:1.1 xlconstant_2 ]
  set_property -dict [ list CONFIG.CONST_VAL {0} CONFIG.CONST_WIDTH {16}  ] $xlconstant_2

  # Create interface connections
  connect_bd_intf_net -intf_net axi_dma_m_axi_mm2s [get_bd_intf_pins axi_dma/M_AXI_MM2S] [get_bd_intf_pins axi_interconnect/S00_AXI]
  connect_bd_intf_net -intf_net axi_dma_m_axi_s2mm [get_bd_intf_pins axi_dma/M_AXI_S2MM] [get_bd_intf_pins axi_interconnect/S01_AXI]
  connect_bd_intf_net -intf_net axi_dma_m_axis_mm2s [get_bd_intf_pins FFT/S_AXIS_DATA] [get_bd_intf_pins axi_dma/M_AXIS_MM2S]
  connect_bd_intf_net -intf_net axi_dma_s_axi_lite [get_bd_intf_pins S_AXI_CTRL] [get_bd_intf_pins axi_dma/S_AXI_LITE]
  connect_bd_intf_net -intf_net axi_interconnect_m00_axi [get_bd_intf_pins M_AXI_MM] [get_bd_intf_pins axi_interconnect/M00_AXI]
  connect_bd_intf_net -intf_net fft_m_axis_data [get_bd_intf_pins FFT/M_AXIS_DATA] [get_bd_intf_pins axi_dma/S_AXIS_S2MM]

  # Create port connections
  connect_bd_net -net aclk [get_bd_pins M_AXI_CLK] [get_bd_pins FFT/aclk] [get_bd_pins axi_dma/m_axi_mm2s_aclk] [get_bd_pins axi_dma/m_axi_s2mm_aclk] [get_bd_pins axi_interconnect/ACLK] [get_bd_pins axi_interconnect/M00_ACLK] [get_bd_pins axi_interconnect/S00_ACLK] [get_bd_pins axi_interconnect/S01_ACLK]
  connect_bd_net -net aresetn [get_bd_pins ARESETN] [get_bd_pins FFT/aresetn] [get_bd_pins axi_dma/axi_resetn] [get_bd_pins axi_interconnect/ARESETN] [get_bd_pins axi_interconnect/M00_ARESETN] [get_bd_pins axi_interconnect/S00_ARESETN] [get_bd_pins axi_interconnect/S01_ARESETN]
  connect_bd_net -net axi_dma_mm2s_introut [get_bd_pins mm2s_introut] [get_bd_pins axi_dma/mm2s_introut]
  connect_bd_net -net axi_dma_s2mm_introut [get_bd_pins s2mm_introut] [get_bd_pins axi_dma/s2mm_introut]
  connect_bd_net -net s_axi_clk_1 [get_bd_pins S_AXI_CLK] [get_bd_pins axi_dma/s_axi_lite_aclk]
  connect_bd_net -net xlconstant_1_const [get_bd_pins FFT/s_axis_config_tvalid] [get_bd_pins xlconstant_1/dout]
  connect_bd_net -net xlconstant_2_dout [get_bd_pins FFT/s_axis_config_tdata] [get_bd_pins xlconstant_2/dout]
 
  # Restore current instance
  current_bd_instance $oldCurInst
}


# Procedure to create entire design; Provide argument to make
# procedure reusable. If parentCell is "", will use root.
proc create_root_design { parentCell } {

  if { $parentCell eq "" } {
     set parentCell [get_bd_cells /]
  }

  # Get object for parentCell
  set parentObj [get_bd_cells $parentCell]
  if { $parentObj == "" } {
     puts "ERROR: Unable to find parent cell <$parentCell>!"
     return
  }

  # Make sure parentObj is hier blk
  set parentType [get_property TYPE $parentObj]
  if { $parentType ne "hier" } {
     puts "ERROR: Parent <$parentObj> has TYPE = <$parentType>. Expected to be <hier>."
     return
  }

  # Save current instance; Restore later
  set oldCurInst [current_bd_instance .]

  # Set parent object as current
  current_bd_instance $parentObj


  # Create interface ports
  set DDR [ create_bd_intf_port -mode Master -vlnv xilinx.com:interface:ddrx_rtl:1.0 DDR ]
  set FIXED_IO [ create_bd_intf_port -mode Master -vlnv xilinx.com:display_processing_system7:fixedio_rtl:1.0 FIXED_IO ]

  # Create ports

  # Create instance: FFT
  create_hier_cell_FFT [current_bd_instance .] FFT

  # Create instance: axi_interconnect_gp0, and set properties
  set axi_interconnect_gp0 [ create_bd_cell -type ip -vlnv xilinx.com:ip:axi_interconnect:2.1 axi_interconnect_gp0 ]
  set_property -dict [ list CONFIG.M06_HAS_REGSLICE {1} CONFIG.NUM_MI {8}  ] $axi_interconnect_gp0

  # Create instance: clk_wiz_1, and set properties
  set clk_wiz_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:clk_wiz:5.1 clk_wiz_1 ]
  set_property -dict [ list CONFIG.CLKOUT1_JITTER {145.943} CONFIG.CLKOUT1_PHASE_ERROR {94.994} CONFIG.CLKOUT1_REQUESTED_OUT_FREQ {50.000} CONFIG.CLKOUT2_JITTER {116.798} CONFIG.CLKOUT2_PHASE_ERROR {94.994} CONFIG.CLKOUT2_REQUESTED_OUT_FREQ {150.000} CONFIG.CLKOUT2_USED {true} CONFIG.NUM_OUT_CLKS {2} CONFIG.PRIM_SOURCE {No_buffer} CONFIG.USE_INCLK_SWITCHOVER {false} CONFIG.USE_RESET {false}  ] $clk_wiz_1

  # Create instance: memory
  create_hier_cell_memory [current_bd_instance .] memory

  # Create instance: proc_sys_reset_1, and set properties
  set proc_sys_reset_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:proc_sys_reset:5.0 proc_sys_reset_1 ]
  set_property -dict [ list CONFIG.C_AUX_RESET_HIGH {0}  ] $proc_sys_reset_1

  # Create instance: processing_system7_1, and set properties
  set processing_system7_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:processing_system7:5.5 processing_system7_1 ]
  set_property -dict [ list CONFIG.PCW_ACT_CAN_PERIPHERAL_FREQMHZ {10.000000}
CONFIG.PCW_ACT_ENET0_PERIPHERAL_FREQMHZ {25.000000} CONFIG.PCW_ACT_ENET1_PERIPHERAL_FREQMHZ {10.000000}
CONFIG.PCW_ACT_FPGA0_PERIPHERAL_FREQMHZ {100.000000} CONFIG.PCW_ACT_FPGA1_PERIPHERAL_FREQMHZ {50.000000}
CONFIG.PCW_ACT_FPGA2_PERIPHERAL_FREQMHZ {50.000000} CONFIG.PCW_ACT_FPGA3_PERIPHERAL_FREQMHZ {50.000000}
CONFIG.PCW_ACT_PCAP_PERIPHERAL_FREQMHZ {200.000000} CONFIG.PCW_ACT_QSPI_PERIPHERAL_FREQMHZ {200.000000}
CONFIG.PCW_ACT_SDIO_PERIPHERAL_FREQMHZ {50.000000} CONFIG.PCW_ACT_SMC_PERIPHERAL_FREQMHZ {10.000000}
CONFIG.PCW_ACT_SPI_PERIPHERAL_FREQMHZ {10.000000} CONFIG.PCW_ACT_TPIU_PERIPHERAL_FREQMHZ {200.000000}
CONFIG.PCW_ACT_UART_PERIPHERAL_FREQMHZ {50.000000} CONFIG.PCW_APU_CLK_RATIO_ENABLE {6:2:1}
CONFIG.PCW_APU_PERIPHERAL_FREQMHZ {666.666666} CONFIG.PCW_CAN0_PERIPHERAL_CLKSRC {External}
CONFIG.PCW_CAN0_PERIPHERAL_ENABLE {0} CONFIG.PCW_CAN1_PERIPHERAL_CLKSRC {External}
CONFIG.PCW_CAN1_PERIPHERAL_ENABLE {0} CONFIG.PCW_CAN_PERIPHERAL_CLKSRC {IO PLL}
CONFIG.PCW_CLK0_FREQ {100000000} CONFIG.PCW_CPU_CPU_6X4X_MAX_RANGE {667}
CONFIG.PCW_CPU_PERIPHERAL_CLKSRC {ARM PLL} CONFIG.PCW_CRYSTAL_PERIPHERAL_FREQMHZ {33.333333}
CONFIG.PCW_DCI_PERIPHERAL_CLKSRC {1} CONFIG.PCW_DCI_PERIPHERAL_FREQMHZ {10.159}
CONFIG.PCW_DDR_PERIPHERAL_CLKSRC {DDR PLL} CONFIG.PCW_DDR_RAM_HIGHADDR {0x3FFFFFFF}
CONFIG.PCW_ENET0_ENET0_IO {MIO 16 .. 27} CONFIG.PCW_ENET0_GRP_MDIO_ENABLE {1}
CONFIG.PCW_ENET0_GRP_MDIO_IO {MIO 52 .. 53} CONFIG.PCW_ENET0_PERIPHERAL_CLKSRC {IO PLL}
CONFIG.PCW_ENET0_PERIPHERAL_ENABLE {1} CONFIG.PCW_ENET0_PERIPHERAL_FREQMHZ {100 Mbps}
CONFIG.PCW_ENET0_RESET_ENABLE {1} CONFIG.PCW_ENET0_RESET_IO {MIO 11}
CONFIG.PCW_ENET1_PERIPHERAL_CLKSRC {IO PLL} CONFIG.PCW_ENET1_PERIPHERAL_ENABLE {0}
CONFIG.PCW_ENET_RESET_POLARITY {Active Low} CONFIG.PCW_EN_4K_TIMER {0}
CONFIG.PCW_EN_CLK0_PORT {1} CONFIG.PCW_EN_CLKTRIG0_PORT {0}
CONFIG.PCW_EN_EMIO_GPIO {1} CONFIG.PCW_EN_EMIO_I2C1 {1}
CONFIG.PCW_EN_ENET0 {1} CONFIG.PCW_EN_GPIO {1}
CONFIG.PCW_EN_I2C0 {1} CONFIG.PCW_EN_I2C1 {1}
CONFIG.PCW_EN_QSPI {1} CONFIG.PCW_EN_RST0_PORT {1}
CONFIG.PCW_EN_SDIO0 {1} CONFIG.PCW_EN_UART1 {1}
CONFIG.PCW_EN_USB0 {1} CONFIG.PCW_FCLK0_PERIPHERAL_CLKSRC {IO PLL}
CONFIG.PCW_FCLK1_PERIPHERAL_CLKSRC {IO PLL} CONFIG.PCW_FCLK2_PERIPHERAL_CLKSRC {IO PLL}
CONFIG.PCW_FCLK3_PERIPHERAL_CLKSRC {IO PLL} CONFIG.PCW_FPGA0_PERIPHERAL_FREQMHZ {100}
CONFIG.PCW_FPGA1_PERIPHERAL_FREQMHZ {50} CONFIG.PCW_FPGA2_PERIPHERAL_FREQMHZ {50}
CONFIG.PCW_FPGA3_PERIPHERAL_FREQMHZ {50} CONFIG.PCW_GPIO_EMIO_GPIO_ENABLE {1}
CONFIG.PCW_GPIO_EMIO_GPIO_IO {2} CONFIG.PCW_GPIO_EMIO_GPIO_WIDTH {2}
CONFIG.PCW_GPIO_MIO_GPIO_ENABLE {1} CONFIG.PCW_GPIO_MIO_GPIO_IO {MIO}
CONFIG.PCW_GPIO_PERIPHERAL_ENABLE {0} CONFIG.PCW_I2C0_GRP_INT_ENABLE {0}
CONFIG.PCW_I2C0_I2C0_IO {MIO 50 .. 51} CONFIG.PCW_I2C0_PERIPHERAL_ENABLE {1}
CONFIG.PCW_I2C0_RESET_ENABLE {1} CONFIG.PCW_I2C0_RESET_IO {MIO 13}
CONFIG.PCW_I2C1_I2C1_IO {EMIO} CONFIG.PCW_I2C1_PERIPHERAL_ENABLE {1}
CONFIG.PCW_I2C_PERIPHERAL_FREQMHZ {111.111115} CONFIG.PCW_I2C_RESET_POLARITY {Active Low}
CONFIG.PCW_IRQ_F2P_INTR {1} CONFIG.PCW_MIO_0_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_0_PULLUP {enabled} CONFIG.PCW_MIO_0_SLEW {slow}
CONFIG.PCW_MIO_10_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_10_PULLUP {enabled}
CONFIG.PCW_MIO_10_SLEW {slow} CONFIG.PCW_MIO_11_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_11_PULLUP {enabled} CONFIG.PCW_MIO_11_SLEW {slow}
CONFIG.PCW_MIO_12_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_12_PULLUP {enabled}
CONFIG.PCW_MIO_12_SLEW {slow} CONFIG.PCW_MIO_13_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_13_PULLUP {enabled} CONFIG.PCW_MIO_13_SLEW {slow}
CONFIG.PCW_MIO_14_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_14_PULLUP {enabled}
CONFIG.PCW_MIO_14_SLEW {slow} CONFIG.PCW_MIO_15_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_15_PULLUP {enabled} CONFIG.PCW_MIO_15_SLEW {slow}
CONFIG.PCW_MIO_16_IOTYPE {HSTL 1.8V} CONFIG.PCW_MIO_16_PULLUP {disabled}
CONFIG.PCW_MIO_16_SLEW {slow} CONFIG.PCW_MIO_17_IOTYPE {HSTL 1.8V}
CONFIG.PCW_MIO_17_PULLUP {disabled} CONFIG.PCW_MIO_17_SLEW {slow}
CONFIG.PCW_MIO_18_IOTYPE {HSTL 1.8V} CONFIG.PCW_MIO_18_PULLUP {disabled}
CONFIG.PCW_MIO_18_SLEW {slow} CONFIG.PCW_MIO_19_IOTYPE {HSTL 1.8V}
CONFIG.PCW_MIO_19_PULLUP {disabled} CONFIG.PCW_MIO_19_SLEW {slow}
CONFIG.PCW_MIO_1_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_1_PULLUP {enabled}
CONFIG.PCW_MIO_1_SLEW {slow} CONFIG.PCW_MIO_20_IOTYPE {HSTL 1.8V}
CONFIG.PCW_MIO_20_PULLUP {disabled} CONFIG.PCW_MIO_20_SLEW {slow}
CONFIG.PCW_MIO_21_IOTYPE {HSTL 1.8V} CONFIG.PCW_MIO_21_PULLUP {disabled}
CONFIG.PCW_MIO_21_SLEW {slow} CONFIG.PCW_MIO_22_IOTYPE {HSTL 1.8V}
CONFIG.PCW_MIO_22_PULLUP {disabled} CONFIG.PCW_MIO_22_SLEW {slow}
CONFIG.PCW_MIO_23_IOTYPE {HSTL 1.8V} CONFIG.PCW_MIO_23_PULLUP {disabled}
CONFIG.PCW_MIO_23_SLEW {slow} CONFIG.PCW_MIO_24_IOTYPE {HSTL 1.8V}
CONFIG.PCW_MIO_24_PULLUP {disabled} CONFIG.PCW_MIO_24_SLEW {slow}
CONFIG.PCW_MIO_25_IOTYPE {HSTL 1.8V} CONFIG.PCW_MIO_25_PULLUP {disabled}
CONFIG.PCW_MIO_25_SLEW {slow} CONFIG.PCW_MIO_26_IOTYPE {HSTL 1.8V}
CONFIG.PCW_MIO_26_PULLUP {disabled} CONFIG.PCW_MIO_26_SLEW {slow}
CONFIG.PCW_MIO_27_IOTYPE {HSTL 1.8V} CONFIG.PCW_MIO_27_PULLUP {disabled}
CONFIG.PCW_MIO_27_SLEW {slow} CONFIG.PCW_MIO_28_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_28_PULLUP {disabled} CONFIG.PCW_MIO_28_SLEW {slow}
CONFIG.PCW_MIO_29_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_29_PULLUP {disabled}
CONFIG.PCW_MIO_29_SLEW {slow} CONFIG.PCW_MIO_2_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_2_SLEW {slow} CONFIG.PCW_MIO_30_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_30_PULLUP {disabled} CONFIG.PCW_MIO_30_SLEW {slow}
CONFIG.PCW_MIO_31_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_31_PULLUP {disabled}
CONFIG.PCW_MIO_31_SLEW {slow} CONFIG.PCW_MIO_32_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_32_PULLUP {disabled} CONFIG.PCW_MIO_32_SLEW {slow}
CONFIG.PCW_MIO_33_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_33_PULLUP {disabled}
CONFIG.PCW_MIO_33_SLEW {slow} CONFIG.PCW_MIO_34_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_34_PULLUP {disabled} CONFIG.PCW_MIO_34_SLEW {slow}
CONFIG.PCW_MIO_35_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_35_PULLUP {disabled}
CONFIG.PCW_MIO_35_SLEW {slow} CONFIG.PCW_MIO_36_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_36_PULLUP {disabled} CONFIG.PCW_MIO_36_SLEW {slow}
CONFIG.PCW_MIO_37_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_37_PULLUP {disabled}
CONFIG.PCW_MIO_37_SLEW {slow} CONFIG.PCW_MIO_38_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_38_PULLUP {disabled} CONFIG.PCW_MIO_38_SLEW {slow}
CONFIG.PCW_MIO_39_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_39_PULLUP {disabled}
CONFIG.PCW_MIO_39_SLEW {slow} CONFIG.PCW_MIO_3_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_3_SLEW {slow} CONFIG.PCW_MIO_40_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_40_PULLUP {disabled} CONFIG.PCW_MIO_40_SLEW {slow}
CONFIG.PCW_MIO_41_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_41_PULLUP {disabled}
CONFIG.PCW_MIO_41_SLEW {slow} CONFIG.PCW_MIO_42_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_42_PULLUP {disabled} CONFIG.PCW_MIO_42_SLEW {slow}
CONFIG.PCW_MIO_43_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_43_PULLUP {disabled}
CONFIG.PCW_MIO_43_SLEW {slow} CONFIG.PCW_MIO_44_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_44_PULLUP {disabled} CONFIG.PCW_MIO_44_SLEW {slow}
CONFIG.PCW_MIO_45_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_45_PULLUP {disabled}
CONFIG.PCW_MIO_45_SLEW {slow} CONFIG.PCW_MIO_46_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_46_PULLUP {enabled} CONFIG.PCW_MIO_46_SLEW {slow}
CONFIG.PCW_MIO_47_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_47_PULLUP {enabled}
CONFIG.PCW_MIO_47_SLEW {slow} CONFIG.PCW_MIO_48_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_48_PULLUP {disabled} CONFIG.PCW_MIO_48_SLEW {slow}
CONFIG.PCW_MIO_49_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_49_PULLUP {disabled}
CONFIG.PCW_MIO_49_SLEW {slow} CONFIG.PCW_MIO_4_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_4_SLEW {slow} CONFIG.PCW_MIO_50_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_50_PULLUP {enabled} CONFIG.PCW_MIO_50_SLEW {slow}
CONFIG.PCW_MIO_51_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_51_PULLUP {enabled}
CONFIG.PCW_MIO_51_SLEW {slow} CONFIG.PCW_MIO_52_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_52_PULLUP {disabled} CONFIG.PCW_MIO_52_SLEW {slow}
CONFIG.PCW_MIO_53_IOTYPE {LVCMOS 1.8V} CONFIG.PCW_MIO_53_PULLUP {disabled}
CONFIG.PCW_MIO_53_SLEW {slow} CONFIG.PCW_MIO_5_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_5_SLEW {slow} CONFIG.PCW_MIO_6_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_6_SLEW {slow} CONFIG.PCW_MIO_7_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_7_SLEW {slow} CONFIG.PCW_MIO_8_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_8_SLEW {slow} CONFIG.PCW_MIO_9_IOTYPE {LVCMOS 1.8V}
CONFIG.PCW_MIO_9_PULLUP {enabled} CONFIG.PCW_MIO_9_SLEW {slow}
CONFIG.PCW_MIO_TREE_PERIPHERALS {SD 0#Quad SPI Flash#Quad SPI Flash#Quad SPI Flash#Quad SPI Flash#Quad SPI Flash#Quad SPI Flash#USB Reset#Quad SPI Flash#GPIO#GPIO#ENET Reset#GPIO#I2C Reset#GPIO#SD 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#Enet 0#USB 0#USB 0#USB 0#USB 0#USB 0#USB 0#USB 0#USB 0#USB 0#USB 0#USB 0#USB 0#SD 0#SD 0#SD 0#SD 0#SD 0#SD 0#GPIO#GPIO#UART 1#UART 1#I2C 0#I2C 0#Enet 0#Enet 0} CONFIG.PCW_MIO_TREE_SIGNALS {cd#qspi0_ss_b#qspi0_io[0]#qspi0_io[1]#qspi0_io[2]#qspi0_io[3]#qspi0_sclk#reset#qspi_fbclk#gpio[9]#gpio[10]#reset#gpio[12]#reset#gpio[14]#wp#tx_clk#txd[0]#txd[1]#txd[2]#txd[3]#tx_ctl#rx_clk#rxd[0]#rxd[1]#rxd[2]#rxd[3]#rx_ctl#data[4]#dir#stp#nxt#data[0]#data[1]#data[2]#data[3]#clk#data[5]#data[6]#data[7]#clk#cmd#data[0]#data[1]#data[2]#data[3]#gpio[46]#gpio[47]#tx#rx#scl#sda#mdc#mdio}
CONFIG.PCW_M_AXI_GP0_FREQMHZ {50} CONFIG.PCW_NAND_CYCLES_T_AR {0}
CONFIG.PCW_NAND_CYCLES_T_CLR {0} CONFIG.PCW_NAND_CYCLES_T_RC {2}
CONFIG.PCW_NAND_CYCLES_T_REA {1} CONFIG.PCW_NAND_CYCLES_T_RR {0}
CONFIG.PCW_NAND_CYCLES_T_WC {2} CONFIG.PCW_NAND_CYCLES_T_WP {1}
CONFIG.PCW_NOR_CS0_T_CEOE {1} CONFIG.PCW_NOR_CS0_T_PC {1}
CONFIG.PCW_NOR_CS0_T_RC {2} CONFIG.PCW_NOR_CS0_T_TR {1}
CONFIG.PCW_NOR_CS0_T_WC {2} CONFIG.PCW_NOR_CS0_T_WP {1}
CONFIG.PCW_NOR_CS0_WE_TIME {2} CONFIG.PCW_NOR_CS1_T_CEOE {1}
CONFIG.PCW_NOR_CS1_T_PC {1} CONFIG.PCW_NOR_CS1_T_RC {2}
CONFIG.PCW_NOR_CS1_T_TR {1} CONFIG.PCW_NOR_CS1_T_WC {2}
CONFIG.PCW_NOR_CS1_T_WP {1} CONFIG.PCW_NOR_CS1_WE_TIME {2}
CONFIG.PCW_NOR_SRAM_CS0_T_CEOE {1} CONFIG.PCW_NOR_SRAM_CS0_T_PC {1}
CONFIG.PCW_NOR_SRAM_CS0_T_RC {2} CONFIG.PCW_NOR_SRAM_CS0_T_TR {1}
CONFIG.PCW_NOR_SRAM_CS0_T_WC {2} CONFIG.PCW_NOR_SRAM_CS0_T_WP {1}
CONFIG.PCW_NOR_SRAM_CS0_WE_TIME {2} CONFIG.PCW_NOR_SRAM_CS1_T_CEOE {1}
CONFIG.PCW_NOR_SRAM_CS1_T_PC {1} CONFIG.PCW_NOR_SRAM_CS1_T_RC {2}
CONFIG.PCW_NOR_SRAM_CS1_T_TR {1} CONFIG.PCW_NOR_SRAM_CS1_T_WC {2}
CONFIG.PCW_NOR_SRAM_CS1_T_WP {1} CONFIG.PCW_NOR_SRAM_CS1_WE_TIME {2}
CONFIG.PCW_PACKAGE_DDR_BOARD_DELAY0 {0.010} CONFIG.PCW_PACKAGE_DDR_BOARD_DELAY1 {0.010}
CONFIG.PCW_PACKAGE_DDR_BOARD_DELAY2 {0.010} CONFIG.PCW_PACKAGE_DDR_BOARD_DELAY3 {0.013}
CONFIG.PCW_PACKAGE_DDR_DQS_TO_CLK_DELAY_0 {-0.001} CONFIG.PCW_PACKAGE_DDR_DQS_TO_CLK_DELAY_1 {-0.002}
CONFIG.PCW_PACKAGE_DDR_DQS_TO_CLK_DELAY_2 {-0.001} CONFIG.PCW_PACKAGE_DDR_DQS_TO_CLK_DELAY_3 {-0.008}
CONFIG.PCW_PCAP_PERIPHERAL_CLKSRC {1} CONFIG.PCW_PCAP_PERIPHERAL_FREQMHZ {200}
CONFIG.PCW_PERIPHERAL_BOARD_PRESET {part0} CONFIG.PCW_PJTAG_PERIPHERAL_ENABLE {0}
CONFIG.PCW_PRESET_BANK0_VOLTAGE {LVCMOS 1.8V} CONFIG.PCW_PRESET_BANK1_VOLTAGE {LVCMOS 1.8V}
CONFIG.PCW_QSPI_GRP_FBCLK_ENABLE {1} CONFIG.PCW_QSPI_GRP_FBCLK_IO {MIO 8}
CONFIG.PCW_QSPI_GRP_IO1_ENABLE {0} CONFIG.PCW_QSPI_GRP_SINGLE_SS_ENABLE {1}
CONFIG.PCW_QSPI_GRP_SINGLE_SS_IO {MIO 1 .. 6} CONFIG.PCW_QSPI_GRP_SS1_ENABLE {0}
CONFIG.PCW_QSPI_PERIPHERAL_CLKSRC {IO PLL} CONFIG.PCW_QSPI_PERIPHERAL_ENABLE {1}
CONFIG.PCW_QSPI_PERIPHERAL_FREQMHZ {200} CONFIG.PCW_QSPI_QSPI_IO {MIO 1 .. 6}
CONFIG.PCW_SD0_GRP_CD_ENABLE {1} CONFIG.PCW_SD0_GRP_CD_IO {MIO 0}
CONFIG.PCW_SD0_GRP_POW_ENABLE {0} CONFIG.PCW_SD0_GRP_WP_ENABLE {1}
CONFIG.PCW_SD0_GRP_WP_IO {MIO 15} CONFIG.PCW_SD0_PERIPHERAL_ENABLE {1}
CONFIG.PCW_SD0_SD0_IO {MIO 40 .. 45} CONFIG.PCW_SD1_PERIPHERAL_ENABLE {0}
CONFIG.PCW_SDIO_PERIPHERAL_CLKSRC {IO PLL} CONFIG.PCW_SDIO_PERIPHERAL_FREQMHZ {50}
CONFIG.PCW_SDIO_PERIPHERAL_VALID {1} CONFIG.PCW_SMC_PERIPHERAL_CLKSRC {IO PLL}
CONFIG.PCW_SPI0_PERIPHERAL_ENABLE {0} CONFIG.PCW_SPI1_PERIPHERAL_ENABLE {0}
CONFIG.PCW_SPI_PERIPHERAL_CLKSRC {IO PLL} CONFIG.PCW_S_AXI_HP0_DATA_WIDTH {64}
CONFIG.PCW_S_AXI_HP0_FREQMHZ {150} CONFIG.PCW_S_AXI_HP2_DATA_WIDTH {64}
CONFIG.PCW_S_AXI_HP2_FREQMHZ {150} CONFIG.PCW_TPIU_PERIPHERAL_CLKSRC {External}
CONFIG.PCW_TRACE_PERIPHERAL_ENABLE {0} CONFIG.PCW_TTC0_CLK0_PERIPHERAL_CLKSRC {CPU_1X}
CONFIG.PCW_TTC0_CLK0_PERIPHERAL_DIVISOR0 {1} CONFIG.PCW_TTC0_CLK1_PERIPHERAL_CLKSRC {CPU_1X}
CONFIG.PCW_TTC0_CLK1_PERIPHERAL_DIVISOR0 {1} CONFIG.PCW_TTC0_CLK2_PERIPHERAL_CLKSRC {CPU_1X}
CONFIG.PCW_TTC0_CLK2_PERIPHERAL_DIVISOR0 {1} CONFIG.PCW_TTC0_PERIPHERAL_ENABLE {0}
CONFIG.PCW_TTC1_CLK0_PERIPHERAL_CLKSRC {CPU_1X} CONFIG.PCW_TTC1_CLK0_PERIPHERAL_DIVISOR0 {1}
CONFIG.PCW_TTC1_CLK1_PERIPHERAL_CLKSRC {CPU_1X} CONFIG.PCW_TTC1_CLK1_PERIPHERAL_DIVISOR0 {1}
CONFIG.PCW_TTC1_CLK2_PERIPHERAL_CLKSRC {CPU_1X} CONFIG.PCW_TTC1_CLK2_PERIPHERAL_DIVISOR0 {1}
CONFIG.PCW_TTC1_PERIPHERAL_ENABLE {0} CONFIG.PCW_UART0_PERIPHERAL_ENABLE {0}
CONFIG.PCW_UART1_BAUD_RATE {115200} CONFIG.PCW_UART1_GRP_FULL_ENABLE {0}
CONFIG.PCW_UART1_PERIPHERAL_ENABLE {1} CONFIG.PCW_UART1_UART1_IO {MIO 48 .. 49}
CONFIG.PCW_UART_PERIPHERAL_CLKSRC {IO PLL} CONFIG.PCW_UART_PERIPHERAL_FREQMHZ {50}
CONFIG.PCW_UIPARAM_DDR_ADV_ENABLE {0} CONFIG.PCW_UIPARAM_DDR_AL {0}
CONFIG.PCW_UIPARAM_DDR_BL {8} CONFIG.PCW_UIPARAM_DDR_BOARD_DELAY0 {0.537}
CONFIG.PCW_UIPARAM_DDR_BOARD_DELAY1 {0.442} CONFIG.PCW_UIPARAM_DDR_BOARD_DELAY2 {0.464}
CONFIG.PCW_UIPARAM_DDR_BOARD_DELAY3 {0.521} CONFIG.PCW_UIPARAM_DDR_BUS_WIDTH {32 Bit}
CONFIG.PCW_UIPARAM_DDR_CLOCK_0_LENGTH_MM {0} CONFIG.PCW_UIPARAM_DDR_CLOCK_0_PACKAGE_LENGTH {61.0905}
CONFIG.PCW_UIPARAM_DDR_CLOCK_0_PROPOGATION_DELAY {160} CONFIG.PCW_UIPARAM_DDR_CLOCK_1_LENGTH_MM {0}
CONFIG.PCW_UIPARAM_DDR_CLOCK_1_PACKAGE_LENGTH {61.0905} CONFIG.PCW_UIPARAM_DDR_CLOCK_1_PROPOGATION_DELAY {160}
CONFIG.PCW_UIPARAM_DDR_CLOCK_2_LENGTH_MM {0} CONFIG.PCW_UIPARAM_DDR_CLOCK_2_PACKAGE_LENGTH {61.0905}
CONFIG.PCW_UIPARAM_DDR_CLOCK_2_PROPOGATION_DELAY {160} CONFIG.PCW_UIPARAM_DDR_CLOCK_3_LENGTH_MM {0}
CONFIG.PCW_UIPARAM_DDR_CLOCK_3_PACKAGE_LENGTH {61.0905} CONFIG.PCW_UIPARAM_DDR_CLOCK_3_PROPOGATION_DELAY {160}
CONFIG.PCW_UIPARAM_DDR_CLOCK_STOP_EN {0} CONFIG.PCW_UIPARAM_DDR_DQS_0_LENGTH_MM {0}
CONFIG.PCW_UIPARAM_DDR_DQS_0_PACKAGE_LENGTH {68.4725} CONFIG.PCW_UIPARAM_DDR_DQS_0_PROPOGATION_DELAY {160}
CONFIG.PCW_UIPARAM_DDR_DQS_1_LENGTH_MM {0} CONFIG.PCW_UIPARAM_DDR_DQS_1_PACKAGE_LENGTH {71.086}
CONFIG.PCW_UIPARAM_DDR_DQS_1_PROPOGATION_DELAY {160} CONFIG.PCW_UIPARAM_DDR_DQS_2_LENGTH_MM {0}
CONFIG.PCW_UIPARAM_DDR_DQS_2_PACKAGE_LENGTH {66.794} CONFIG.PCW_UIPARAM_DDR_DQS_2_PROPOGATION_DELAY {160}
CONFIG.PCW_UIPARAM_DDR_DQS_3_LENGTH_MM {0} CONFIG.PCW_UIPARAM_DDR_DQS_3_PACKAGE_LENGTH {108.7385}
CONFIG.PCW_UIPARAM_DDR_DQS_3_PROPOGATION_DELAY {160} CONFIG.PCW_UIPARAM_DDR_DQS_TO_CLK_DELAY_0 {0.217}
CONFIG.PCW_UIPARAM_DDR_DQS_TO_CLK_DELAY_1 {0.133} CONFIG.PCW_UIPARAM_DDR_DQS_TO_CLK_DELAY_2 {0.089}
CONFIG.PCW_UIPARAM_DDR_DQS_TO_CLK_DELAY_3 {0.248} CONFIG.PCW_UIPARAM_DDR_DQ_0_LENGTH_MM {0}
CONFIG.PCW_UIPARAM_DDR_DQ_0_PACKAGE_LENGTH {64.1705} CONFIG.PCW_UIPARAM_DDR_DQ_0_PROPOGATION_DELAY {160}
CONFIG.PCW_UIPARAM_DDR_DQ_1_LENGTH_MM {0} CONFIG.PCW_UIPARAM_DDR_DQ_1_PACKAGE_LENGTH {63.686}
CONFIG.PCW_UIPARAM_DDR_DQ_1_PROPOGATION_DELAY {160} CONFIG.PCW_UIPARAM_DDR_DQ_2_LENGTH_MM {0}
CONFIG.PCW_UIPARAM_DDR_DQ_2_PACKAGE_LENGTH {68.46} CONFIG.PCW_UIPARAM_DDR_DQ_2_PROPOGATION_DELAY {160}
CONFIG.PCW_UIPARAM_DDR_DQ_3_LENGTH_MM {0} CONFIG.PCW_UIPARAM_DDR_DQ_3_PACKAGE_LENGTH {105.4895}
CONFIG.PCW_UIPARAM_DDR_DQ_3_PROPOGATION_DELAY {160} CONFIG.PCW_UIPARAM_DDR_ENABLE {1}
CONFIG.PCW_UIPARAM_DDR_FREQ_MHZ {533.333333} CONFIG.PCW_UIPARAM_DDR_HIGH_TEMP {Normal (0-85)}
CONFIG.PCW_UIPARAM_DDR_MEMORY_TYPE {DDR 3} CONFIG.PCW_UIPARAM_DDR_PARTNO {MT41J256M8 HX-15E}
CONFIG.PCW_UIPARAM_DDR_TRAIN_DATA_EYE {1} CONFIG.PCW_UIPARAM_DDR_TRAIN_READ_GATE {1}
CONFIG.PCW_UIPARAM_DDR_TRAIN_WRITE_LEVEL {1} CONFIG.PCW_UIPARAM_DDR_USE_INTERNAL_VREF {1}
CONFIG.PCW_USB0_PERIPHERAL_ENABLE {1} CONFIG.PCW_USB0_RESET_ENABLE {1}
CONFIG.PCW_USB0_RESET_IO {MIO 7} CONFIG.PCW_USB0_USB0_IO {MIO 28 .. 39}
CONFIG.PCW_USB1_PERIPHERAL_ENABLE {0} CONFIG.PCW_USB_RESET_POLARITY {Active Low}
CONFIG.PCW_USE_CROSS_TRIGGER {0} CONFIG.PCW_USE_DEFAULT_ACP_USER_VAL {1}
CONFIG.PCW_USE_FABRIC_INTERRUPT {1} CONFIG.PCW_USE_HIGH_OCM {1}
CONFIG.PCW_USE_M_AXI_GP0 {1} CONFIG.PCW_USE_S_AXI_ACP {1}
CONFIG.PCW_USE_S_AXI_HP0 {1} CONFIG.PCW_USE_S_AXI_HP1 {0}
CONFIG.PCW_USE_S_AXI_HP2 {1} CONFIG.PCW_WDT_PERIPHERAL_CLKSRC {CPU_1X}
CONFIG.PCW_WDT_PERIPHERAL_DIVISOR0 {1} CONFIG.PCW_WDT_PERIPHERAL_ENABLE {0}
CONFIG.preset {ZC702*}  ] $processing_system7_1

  # Create instance: xlconcat_1, and set properties
  set xlconcat_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:xlconcat:2.1 xlconcat_1 ]
  set_property -dict [ list CONFIG.NUM_PORTS {9}  ] $xlconcat_1

  # Create instance: xlconstant_1, and set properties
  set xlconstant_1 [ create_bd_cell -type ip -vlnv xilinx.com:ip:xlconstant:1.1 xlconstant_1 ]
  set_property -dict [ list CONFIG.CONST_VAL {0}  ] $xlconstant_1

  # Create interface connections
  connect_bd_intf_net -intf_net FFT_M_AXI_MM [get_bd_intf_pins FFT/M_AXI_MM] [get_bd_intf_pins processing_system7_1/S_AXI_ACP]
  connect_bd_intf_net -intf_net axi4_gp0_M03_AXI [get_bd_intf_pins axi_interconnect_gp0/M03_AXI] [get_bd_intf_pins memory/S_AXI]
  connect_bd_intf_net -intf_net axi_interconnect_1_m00_axi [get_bd_intf_pins memory/M00_AXI] [get_bd_intf_pins processing_system7_1/S_AXI_HP0]
  connect_bd_intf_net -intf_net axi_interconnect_3_m00_axi [get_bd_intf_pins memory/M00_AXI1] [get_bd_intf_pins processing_system7_1/S_AXI_HP2]
  connect_bd_intf_net -intf_net axi_interconnect_gp0_M01_AXI [get_bd_intf_pins axi_interconnect_gp0/M01_AXI] [get_bd_intf_pins memory/S_AXI_LITE1]
  connect_bd_intf_net -intf_net axi_interconnect_gp0_M02_AXI [get_bd_intf_pins axi_interconnect_gp0/M02_AXI] [get_bd_intf_pins memory/S_AXI_LITE]
  connect_bd_intf_net -intf_net axi_interconnect_gp0_M07_AXI [get_bd_intf_pins FFT/S_AXI_CTRL] [get_bd_intf_pins axi_interconnect_gp0/M07_AXI]
  connect_bd_intf_net -intf_net processing_system7_1_ddr [get_bd_intf_ports DDR] [get_bd_intf_pins processing_system7_1/DDR]
  connect_bd_intf_net -intf_net processing_system7_1_fixed_io [get_bd_intf_ports FIXED_IO] [get_bd_intf_pins processing_system7_1/FIXED_IO]
  connect_bd_intf_net -intf_net s00_axi_1 [get_bd_intf_pins axi_interconnect_gp0/S00_AXI] [get_bd_intf_pins processing_system7_1/M_AXI_GP0]

  # Create port connections
  connect_bd_net -net FFT_mm2s_introut [get_bd_pins FFT/mm2s_introut] [get_bd_pins xlconcat_1/In7]
  connect_bd_net -net FFT_s2mm_introut [get_bd_pins FFT/s2mm_introut] [get_bd_pins xlconcat_1/In8]
  connect_bd_net -net clk_150mhz [get_bd_pins FFT/M_AXI_CLK] [get_bd_pins axi_interconnect_gp0/M06_ACLK] [get_bd_pins clk_wiz_1/clk_out2] [get_bd_pins memory/core_aclk] [get_bd_pins processing_system7_1/S_AXI_ACP_ACLK] [get_bd_pins processing_system7_1/S_AXI_HP0_ACLK] [get_bd_pins processing_system7_1/S_AXI_HP2_ACLK]
  connect_bd_net -net clk_75mhz [get_bd_pins FFT/S02_ACLK] [get_bd_pins FFT/S_AXI_CLK] [get_bd_pins axi_interconnect_gp0/ACLK] [get_bd_pins axi_interconnect_gp0/M00_ACLK] [get_bd_pins axi_interconnect_gp0/M01_ACLK] [get_bd_pins axi_interconnect_gp0/M02_ACLK] [get_bd_pins axi_interconnect_gp0/M03_ACLK] [get_bd_pins axi_interconnect_gp0/M04_ACLK] [get_bd_pins axi_interconnect_gp0/M05_ACLK] [get_bd_pins axi_interconnect_gp0/M07_ACLK] [get_bd_pins axi_interconnect_gp0/S00_ACLK] [get_bd_pins clk_wiz_1/clk_out1] [get_bd_pins memory/s_axi_aclk] [get_bd_pins proc_sys_reset_1/slowest_sync_clk] [get_bd_pins processing_system7_1/M_AXI_GP0_ACLK]
  connect_bd_net -net clk_wiz_1_locked [get_bd_pins clk_wiz_1/locked] [get_bd_pins proc_sys_reset_1/dcm_locked]
  connect_bd_net -net filter_vdma_mm2s_int_1 [get_bd_pins memory/mm2s_introut] [get_bd_pins xlconcat_1/In2]
  connect_bd_net -net filter_vdma_s2mm_int_1 [get_bd_pins memory/s2mm_introut] [get_bd_pins xlconcat_1/In3]
  connect_bd_net -net memory_PerfMon_intr [get_bd_pins memory/PerfMon_intr] [get_bd_pins xlconcat_1/In6]
  connect_bd_net -net proc_sys_reset_1_interconnect_aresetn [get_bd_pins FFT/ARESETN] [get_bd_pins FFT/S02_ARESETN] [get_bd_pins axi_interconnect_gp0/ARESETN] [get_bd_pins axi_interconnect_gp0/M00_ARESETN] [get_bd_pins axi_interconnect_gp0/M01_ARESETN] [get_bd_pins axi_interconnect_gp0/M02_ARESETN] [get_bd_pins axi_interconnect_gp0/M03_ARESETN] [get_bd_pins axi_interconnect_gp0/M04_ARESETN] [get_bd_pins axi_interconnect_gp0/M05_ARESETN] [get_bd_pins axi_interconnect_gp0/M06_ARESETN] [get_bd_pins axi_interconnect_gp0/M07_ARESETN] [get_bd_pins axi_interconnect_gp0/S00_ARESETN] [get_bd_pins memory/core_aresetn] [get_bd_pins proc_sys_reset_1/interconnect_aresetn]
  connect_bd_net -net processing_system7_1_fclk_clk0 [get_bd_pins clk_wiz_1/clk_in1] [get_bd_pins processing_system7_1/FCLK_CLK0]
  connect_bd_net -net processing_system7_1_fclk_reset0_n [get_bd_pins proc_sys_reset_1/ext_reset_in] [get_bd_pins processing_system7_1/FCLK_RESET0_N]
  connect_bd_net -net tpg_vdma_s2mm_int_1 [get_bd_pins memory/s2mm_introut1] [get_bd_pins xlconcat_1/In4]
  connect_bd_net -net xlconcat_1_dout [get_bd_pins processing_system7_1/IRQ_F2P] [get_bd_pins xlconcat_1/dout]
  connect_bd_net -net xlconstant_1_dout [get_bd_pins xlconcat_1/In0] [get_bd_pins xlconcat_1/In1] [get_bd_pins xlconcat_1/In5] [get_bd_pins xlconstant_1/dout]

  # Create address segments
  create_bd_addr_seg -range 0x10000 -offset 0x40090000 [get_bd_addr_spaces processing_system7_1/Data] [get_bd_addr_segs memory/axi_vdma_1/S_AXI_LITE/Reg] SEG2
  create_bd_addr_seg -range 0x10000 -offset 0x400B0000 [get_bd_addr_spaces processing_system7_1/Data] [get_bd_addr_segs memory/axi_vdma_2/S_AXI_LITE/Reg] SEG_FILTER_VDMA_Reg
  create_bd_addr_seg -range 0x10000 -offset 0x400F0000 [get_bd_addr_spaces processing_system7_1/Data] [get_bd_addr_segs memory/axi_perf_mon_1/S_AXI/Reg] SEG_PERF_MON_HP0_HP2_Reg
  create_bd_addr_seg -range 0x10000 -offset 0x40400000 [get_bd_addr_spaces processing_system7_1/Data] [get_bd_addr_segs FFT/axi_dma/S_AXI_LITE/Reg] SEG_axi_dma_Reg
  create_bd_addr_seg -range 0x40000000 -offset 0x0 [get_bd_addr_spaces FFT/axi_dma/Data_MM2S] [get_bd_addr_segs processing_system7_1/S_AXI_ACP/ACP_DDR_LOWOCM] SEG_processing_system7_1_ACP_DDR_LOWOCM
  create_bd_addr_seg -range 0x40000000 -offset 0x0 [get_bd_addr_spaces FFT/axi_dma/Data_S2MM] [get_bd_addr_segs processing_system7_1/S_AXI_ACP/ACP_DDR_LOWOCM] SEG_processing_system7_1_ACP_DDR_LOWOCM
  create_bd_addr_seg -range 0x40000 -offset 0xFFFC0000 [get_bd_addr_spaces FFT/axi_dma/Data_MM2S] [get_bd_addr_segs processing_system7_1/S_AXI_ACP/ACP_HIGH_OCM] SEG_processing_system7_1_ACP_HIGH_OCM
  create_bd_addr_seg -range 0x40000 -offset 0xFFFC0000 [get_bd_addr_spaces FFT/axi_dma/Data_S2MM] [get_bd_addr_segs processing_system7_1/S_AXI_ACP/ACP_HIGH_OCM] SEG_processing_system7_1_ACP_HIGH_OCM
  create_bd_addr_seg -range 0x40000000 -offset 0x0 [get_bd_addr_spaces memory/axi_vdma_1/Data_S2MM] [get_bd_addr_segs processing_system7_1/S_AXI_HP0/HP0_DDR_LOWOCM] SEG_processing_system7_1_HP0_DDR_LOWOCM
  create_bd_addr_seg -range 0x40000000 -offset 0x0 [get_bd_addr_spaces memory/axi_vdma_2/Data_MM2S] [get_bd_addr_segs processing_system7_1/S_AXI_HP2/HP2_DDR_LOWOCM] SEG1
  create_bd_addr_seg -range 0x40000000 -offset 0x0 [get_bd_addr_spaces memory/axi_vdma_2/Data_S2MM] [get_bd_addr_segs processing_system7_1/S_AXI_HP2/HP2_DDR_LOWOCM] SEG2
 

  # Restore current instance
  current_bd_instance $oldCurInst

  save_bd_design
}
# End of create_root_design()


##################################################################
# MAIN FLOW
##################################################################

create_root_design ""


  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hello Max,

     

    I did not go through the complete design but I did notice two things. One is that you are using a different version of Vivado and PetaLinux than the project was done in. I would suggest using the same tools version as the original project at least to get started.

     

    Also, are you sure that you have removed all of the portions of the design that are supported by the ZC702 hardware but not present on the MicroZed? I did notice an I2C peripheral listed but there is no I2C peripheral on the basic MicroZed as there is on the ZC702 board. Also, did you check that all of the MIO connections are modified as needed?

     

    -Gary