Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Making the XADC read an external value
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 362 subscribers
  • Views 979 views
  • Users 0 members are here
Related

Making the XADC read an external value

e14 Contributor
e14 Contributor over 11 years ago

Hello, guys.
I've been working with microzed attached to a IO carrier board, and trying to read a voltage input in a channel.
Problem is: all the starter-microzed guides uses XADC to read internal values. Therefore, I don't have any material on which I can rely.
In vivado, i'm using a processor IP, an axi interconnect and an xadc_wiz. I don't even know where should I plug the xadc's  P and N outputs.
Do anybody have a model for this kind of application, since i'm completely lost in my task?
Thanks!

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    This forum post discusses using the XADC, including connecting to external signals:

     

    http://zedboard.org/content/xilinx-xadc

     

    It references this blog,  lab 3 looks to be helpful: http://zynqhowto.blogspot.kr/

     

    Once you have built your Vivado design and selected the IO from the carrier card you can use/modify the master constraints file available for download on the carrier card's document page. This is the page for the MicroZed IO Carrier Card: http://zedboard.org/support/documentation/1522

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 9 years ago

    sir I need help in XADC portion. I am using zedboard and vivado i need to convert two voltage signal coming from solar simulator into digital value.I have tried alot but didn't getting result. I am trying with IP catlog XADC DRP I selecting two channels Vp0 and Vp 8 but how i get simultanious result.i need result in some register so i can use that register in my further project.THANKS

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 9 years ago

    Hi Sumans,

    The most I can offer you are the links that Gary provided above along with this post.

    https://forums.xilinx.com/t5/Xcell-Daily-Blog/Getting-the-XADC-Running-on-the-MicroZed-Adam-Taylor-s-MicroZed/ba-p/380989

    For any future assistance I am going to ask that you post over at the Digilent forum as they are the main point of contact for educational support.

    https://forum.digilentinc.com/

    Thanks,

    Josh