Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed 7010 Sluggish response
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 363 subscribers
  • Views 1295 views
  • Users 0 members are here
Related

Microzed 7010 Sluggish response

100bobdxcool
100bobdxcool over 10 years ago

I have ubuntu based OS (xillinux) installed on my zynq 7010 based microzed board (commercial version) and having certain scripts running on them outdoors. I have 10 such systems outdoors. But only on two particular systems, whenever I login to these system, the response from the terminal is very sluggish and CPU itself seems to be running slow. After I reboot the system, then it would start running normally, and then again after a few hours, shows up the same behavior. What could be the possible reasons for this ?

Some process is utilizing maximum CPU resources ?
Or the 8GB SD card quality isnt good (Currently using the SD card that came with the microzed kit) ? What SD card is recommended to be used if so ?

What else could be the issue ? Temperature (Currently the microzed sits on my custom designed PCB which is usually at a temperature of 30-35 C based on the temperature sensor I have on board)  ?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    As usual, I recommend Sandisk. I have no experience with the other brands, but the difference in price is probably small, and Sandisk has a long track record.

    Running a filesystem on the SD is by far more demanding than its intended use (camera / cellular data storage): The OS constantly writes small pieces of data to the flash disk, so just by having the OS running, it's constantly being worn out.

    A factor that is often overlooked is Write Amplification (WA):

    https://en.wikipedia.org/wiki/Write_amplification

    What Wikipedia doesn't emphasize enough is that the most important factor in keeping the WA down is that the SSD controller knows which write operation contains metadata that is likely to be overwritten soon, an which is constant data. This knowledge allows it to pack the written data in an efficient way.

    It's a known secret that good SSD controllers detect the filesystem for this purpose. There's a reason they all arrive formatted with FAT32 (which is the most used), but the good ones work well with a variety of other filesystems. The difference between brands is not so much the flash memory itself, but the SSD controller's ability to keep the WA down by making good guesses on what kind of data is being written.

    My hunch is that Sandisk flashes have an SSD that recognizes ext2/3/4 file system while others don't. That's probably why Sandisk works so well with Xillinux, and other flashes fail so soon.

    A swap partition is completely unnecessary. And it would kill the flash device quite rapidly if it became necessary, as its content and read/write pattern is completely random.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello,

    As usual, I recommend Sandisk. I have no experience with the other brands, but the difference in price is probably small, and Sandisk has a long track record.

    Running a filesystem on the SD is by far more demanding than its intended use (camera / cellular data storage): The OS constantly writes small pieces of data to the flash disk, so just by having the OS running, it's constantly being worn out.

    A factor that is often overlooked is Write Amplification (WA):

    https://en.wikipedia.org/wiki/Write_amplification

    What Wikipedia doesn't emphasize enough is that the most important factor in keeping the WA down is that the SSD controller knows which write operation contains metadata that is likely to be overwritten soon, an which is constant data. This knowledge allows it to pack the written data in an efficient way.

    It's a known secret that good SSD controllers detect the filesystem for this purpose. There's a reason they all arrive formatted with FAT32 (which is the most used), but the good ones work well with a variety of other filesystems. The difference between brands is not so much the flash memory itself, but the SSD controller's ability to keep the WA down by making good guesses on what kind of data is being written.

    My hunch is that Sandisk flashes have an SSD that recognizes ext2/3/4 file system while others don't. That's probably why Sandisk works so well with Xillinux, and other flashes fail so soon.

    A swap partition is completely unnecessary. And it would kill the flash device quite rapidly if it became necessary, as its content and read/write pattern is completely random.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • 100bobdxcool
    0 100bobdxcool over 10 years ago in reply to e14 Contributor

    Is something like sandisk ultimate or sandisk extreme recommended for use for my application as my application runs 24x7 (and so was thinking if it was better to have an industrial grade SD card) ? And also xillinux can support maximum 64gb Sandisk SD card ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to 100bobdxcool

    Hi,

    I've actually had a good experience running a simple data logging program for about a year 24/7 on a Zybo card, with plain Xillinux. The program itself didn't write much, but anyhow -- there were no issues with the SD card.

    So a plain and simple 8 GB card from Sandisk is probably the best choice. Larger cards may be less reliable, and I don't recommend industrial grade versions unless you're outside the commercial temperature range. Industrial products are less commonly used, and are often less reliable within the working conditions ranges that are supported by commercial versions.

    Alternatively, you may try to run Xillinux (or another distribution, for that matter) with the root filesystem mounted read-only. On top of that, mount another partition (possibly FAT32 or ext4, but not encrypted or some loop mount) for the application data you need to save on the card.

    This way you'll keep the amount of writes to what you actually need. But odds are that even that won't be necessary.

    Regards,
       Eli

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100bobdxcool
    0 100bobdxcool over 10 years ago in reply to e14 Contributor

    I also use the system for writing logs and for communication regularly with a server. The system scripts get updated like once a month through git.

    Also, regarding mounting the root partition as read only and another partition for storing scripts and logs, can you please suggest me on how to do this (any lins would be helpful) ? I beleive xillinux already uses two partitions.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100bobdxcool
    0 100bobdxcool over 10 years ago in reply to e14 Contributor

    Can you please help me on how to mount the root file system as read only and also create a application data partition ?