Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Boot from USB Thumb Drive
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 343 views
  • Users 0 members are here
Related

Boot from USB Thumb Drive

e14 Contributor
e14 Contributor over 11 years ago

Is it possible to use the built-in USB port to boot and configure the Microzed, instead of using the micro sd-card port?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Not directly. The first stage boot image has to come from QSPI, SD Card, NOR or NAND Flash in Master Boot mode or from JTAG in Slave Boot mode (see chapter 6 of the Zynq TRM http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf ).

     

    Since the MicroZed does not have NAND or NOR Flash that limits Master Boot mode to QSPI or micro SD Card. You do have the option to load a second stage boot loader program (i.e. U-Boot) from QSPI or the microSD Card and have that load the remainder of your OS or code from USB.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Not directly. The first stage boot image has to come from QSPI, SD Card, NOR or NAND Flash in Master Boot mode or from JTAG in Slave Boot mode (see chapter 6 of the Zynq TRM http://www.xilinx.com/support/documentation/user_guides/ug585-Zynq-7000-TRM.pdf ).

     

    Since the MicroZed does not have NAND or NOR Flash that limits Master Boot mode to QSPI or micro SD Card. You do have the option to load a second stage boot loader program (i.e. U-Boot) from QSPI or the microSD Card and have that load the remainder of your OS or code from USB.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer