Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design using microzed board with 2017.4
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 7 replies
  • Subscribers 362 subscribers
  • Views 1192 views
  • Users 0 members are here
Related

using microzed board with 2017.4

roymesi
roymesi over 8 years ago

In this link:

http://zedboard.org/support/documentation/1519

I've seen 'board definition files' only for versions which are prior to last release 2017.4 (e.g., 2016.4 and below). 

Can I use these files also with 2017.4?

Same question goes for the tcl files in this link.

Thanks.

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 8 years ago

    Yes, those board definitions and TCL files should work in any version of 2017.x. We need to update the label on our website.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago

    Hello,

    I have just downloaded the latest uZed board definition file:

                  Avnet Zed Board Defnition Files.zip                                                     (is)

    and compared with previous: 

                  Avnet Zed Board Definitions 2015_3or4_2016_1or2_160826_3.zip   (was)

     

    But I have found differences not reflected in Revision History (file preset.xml \ 1.1 , for both 7010, 7020):

     

    was:

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_0_LENGTH_MM" value="39.7"

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_1_LENGTH_MM" value="39.7"

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_2_LENGTH_MM" value="54.14"

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_3_LENGTH_MM" value="54.14"

     

    is:

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_0_LENGTH_MM" value="54.14"

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_1_LENGTH_MM" value="54.14"

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_2_LENGTH_MM" value="39.7"

    user_parameter name="CONFIG.PCW_UIPARAM_DDR_CLOCK_3_LENGTH_MM" value="39.7"

     

    So track lengths are swapped.

    Which is correct ?

     

    I have to maintenance the uZed as old as rev. F01.

    May I use the same board definitions for those old F01 and the uZed of the latest revisions?

     

    Thank you in advance for help.

     

    Regards

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Robert,

    This forum post should solve your question.

    http://zedboard.org/content/novice-zynq-ddr3-memory-controller

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to jafoste4

    Hello Josh,

    thank you very much for this link. It is really impressive !

    I would like to make a little clearance...

    I guess that the Board Definitions I have just downloaded (dated 2018-01-01) is the best already known and suitable for uZed ver. G , isn't it ?

    But I have also to maintenance uZed ver. F01. May I assume that this latest version is suitable for uZed as old as F01?  Or I should take an older "Board Definitions"?

    Regards

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Robert,

    The Board Definition File dated (2018-01-01) is the suggested board definition file to be used regardless of uZed version.

    So to answer your question, yes the 2018-01-01 version can/should be used with your uZed F01.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 8 years ago in reply to jafoste4

    Hello Josh,

    many thanks for this reply.

    Sorry for such a simple question but after investigation of a few versions I got doubts.

    Thanks again

    Robert

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Robert,

    No worries! Its always better to double check. Please post again if you encounter any further issues.

    Thanks,
    Josh