Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed I2C clock speed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 360 subscribers
  • Views 849 views
  • Users 0 members are here
Related

Microzed I2C clock speed

e14 Contributor
e14 Contributor over 8 years ago

Does anybody have any idea how to set the clock frequency of the PS I2C interface of a microzed running petalinux? Ideally this could be done by an application at runtime but this appears not to be possible.

The only way I have found to do it is to manually edit the pcw.dtsi files created by petalinux-config.

The relevant line is

    clock-frequency = <400000>;

That is not really satisfactory as one day I'll make a change and forget and my devices will fail in the field.

And on a related topic, when I do set it to 400000 I get 285kHz. When I set it to 100000 I get 90kHz. Setting it to 250000 gives you 196kHz. I realise that there are only integer dividers so not all frequencies are possible but my calcs suggest we should get a lot closer. 

  • Sign in to reply
  • Cancel
  • bhfletcher
    0 bhfletcher over 8 years ago

    Hello @dbbt,

    It sounds like this is not specific to the MicroZed but rather something specific to Zynq-7000 and the Cadence PS I2C hardware and driver. You should definitely request this information on the Xilinx forums as they have detailed product experts who can help as well.

    I did a bit of searching to get you started, and it looks like you are not the only one having similar issues. Check these out, and then I'd encourage you to open your own forum post with Xilinx.

    https://forums.xilinx.com/t5/Embedded-Linux/i2c-cadence-driver-frequency-in-petalinux/td-p/744270

    https://forums.xilinx.com/t5/Embedded-Development-Tools/Petalinux-2016-4-I2C-problem/td-p/788464

    https://forums.xilinx.com/t5/Embedded-Linux/Cadence-I2C-Clock-Frequency/td-p/759420

    https://forums.xilinx.com/t5/Embedded-Processor-System-Design/Adjust-I2C-clock-on-iic0-interface/td-p/562906

     

    Bryan