Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Adapting a Zedboard code to Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 598 views
  • Users 0 members are here
Related

Adapting a Zedboard code to Microzed

e14 Contributor
e14 Contributor over 11 years ago

Hi!
I've been doing some experimentation with MicroZed recently, but I only found guides about what I'm trying to do applied to the Zedboard.
Apart from Vivado, what are the SDK nuances I need to look at in order to make my C code run in the Microzed board?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    There are some differences between the two boards.

     

    The ZedBoard has a Zynq 7020 device. MicroZed may have a Zynq 7010 or 7020 device, depending on the version you have. So, if you have the 7010 version of the MicroZed it will have less Programmable Logic resources and less internal BRAM, if you have the 7020 version then ZedBoard and MicroZed have the same internal resources. The device on the MicroZed is in a smaller package with fewer I/O pins.

     

    Both versions of the MicroZed have 1 GB of DDR memory, twice that of the ZedBoard.

    The ZedBoard has an SD Card socket and 256 Mb of QSPI Flash while the MicroZed has a microSD card socket and 128 Mb of QSPI Flash.

     

    There are other obvious differences in the connections available, such as PMOD connections and LPC FMC connector unless you are using a Carrier Card with the MicroZed. You should make sure that any peripheral devices you plan to use, such as I2S and HDMI/VGA interfaces that are on the ZedBoard are on a carrier card for the MicroZed.

     

    Otherwise, from an SDK point of view not many differences. You will need to 'export' your MicroZed hardware to the SDK and rebuild a new BSP. Then, assuming all of the peripherals and drivers are there, your code should run on the MicroZed.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hey, Gary!
    Thank you for your kind answer.
    I'm using MicroZed with a carrier board.
    I've been trying to apply a XADC voltage reader, and found a Zedboard Guide. Everything seems right in vivado (wiring in block diagram, constraints, ports, etc), but when I use the C code in SDK it just doesn't work.
    I'm afraid it is something involving the constraints code and/or a problem with drivers/includes in the SDK code.
    I've been trying to check all the code with ZYNQ documentations, but can't find whats wrong.
    The guide (pdf) I previously commented is on this link:
    https://docs.google.com/viewer?a=v&pid=sites&srcid=ZGVmYXVsdGRvbWFpbnxydGNsYWIwOXxneDoyYTgxZDNjMmVjZjRmZmVm
    Can someone please help me finding out what is the difference?
    I know that's an easy task, but since I'm new to this subject, this is really bugging me out.
    Thanks in advance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Hey, Gary!
    Thank you for your kind answer.
    I'm using MicroZed with a carrier board.
    I've been trying to apply a XADC voltage reader, and found a Zedboard Guide. Everything seems right in vivado (wiring in block diagram, constraints, ports, etc), but when I use the C code in SDK it just doesn't work.
    I'm afraid it is something involving the constraints code and/or a problem with drivers/includes in the SDK code.
    I've been trying to check all the code with ZYNQ documentations, but can't find whats wrong.
    The guide (pdf) I previously commented is on this link:
    https://docs.google.com/viewer?a=v&pid=sites&srcid=ZGVmYXVsdGRvbWFpbnxydGNsYWIwOXxneDoyYTgxZDNjMmVjZjRmZmVm
    Can someone please help me finding out what is the difference?
    I know that's an easy task, but since I'm new to this subject, this is really bugging me out.
    Thanks in advance.