Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Adapting a Zedboard code to Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 598 views
  • Users 0 members are here
Related

Adapting a Zedboard code to Microzed

e14 Contributor
e14 Contributor over 11 years ago

Hi!
I've been doing some experimentation with MicroZed recently, but I only found guides about what I'm trying to do applied to the Zedboard.
Apart from Vivado, what are the SDK nuances I need to look at in order to make my C code run in the Microzed board?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You will need to change the constraints file to match the different Zynq package pin/signals between the ZedBoard and the MicroZed as the two boards have different Zynq packages. I am not familiar with the lab material you refer to, and the constraints file is not available on your linked file, so I can't give you specific changes to make. Take a look at the MicroZed master .xdc files available on the MicroZed documentation page: http://zedboard.org/support/documentation/1519 and the MicroZed Carrier Card documentation pages: 

    http://zedboard.org/support/documentation/2180

    http://zedboard.org/support/documentation/1522

    http://zedboard.org/support/documentation/2182

    depending on which Carrier Card you are using.

     

    There is also a bug in Vivado 2014.4 that causes IO Buffers to be inferred for some of the XADC signals that did not occur in previous Vivado versions. So some location constraints that did not have to be explicitly added to your .xdc file in other versions of Vivado do need to be added in 2014.4. This would cause an error in your Vivado Hardware project though, so if you are able to generate and export your design to SDK successfully that is not your issue. (see this forum post for details): 

    http://zedboard.org/content/vivado-20144-microzed-incompatible-board-definition-file

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    You will need to change the constraints file to match the different Zynq package pin/signals between the ZedBoard and the MicroZed as the two boards have different Zynq packages. I am not familiar with the lab material you refer to, and the constraints file is not available on your linked file, so I can't give you specific changes to make. Take a look at the MicroZed master .xdc files available on the MicroZed documentation page: http://zedboard.org/support/documentation/1519 and the MicroZed Carrier Card documentation pages: 

    http://zedboard.org/support/documentation/2180

    http://zedboard.org/support/documentation/1522

    http://zedboard.org/support/documentation/2182

    depending on which Carrier Card you are using.

     

    There is also a bug in Vivado 2014.4 that causes IO Buffers to be inferred for some of the XADC signals that did not occur in previous Vivado versions. So some location constraints that did not have to be explicitly added to your .xdc file in other versions of Vivado do need to be added in 2014.4. This would cause an error in your Vivado Hardware project though, so if you are able to generate and export your design to SDK successfully that is not your issue. (see this forum post for details): 

    http://zedboard.org/content/vivado-20144-microzed-incompatible-board-definition-file

     

    -Gary