Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Adding second SD Card to Zedboard PMOD
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 655 views
  • Users 0 members are here
Related

Adding second SD Card to Zedboard PMOD

e14 Contributor
e14 Contributor over 12 years ago

I am trying to add a second SD card P/N PMODSD (link at the bottom) to the Zedboard using one of the PMOD connectors. I know the SD card built into the Zedboard connects directly into the Processing System of the Zedboard and MIO connectors therefore does that mean to add in another SD card I would have to use the PMOD connected to the PS. Or can I use any of the four PMODs connected to the PL side of the Zedboard?

Secondly, if is possibly to add another SD card to the Zedboard, is there any downloadable configurations available already for an SPI communication PMOD? Is there any code available so I can just configure into my LINUX platform and connect directly to the PMOD SD card?

http://www.digilentinc.com/Products/Detail.cfm?NavPath=2,401,513&Prod=PMOD-SD

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    I can see how the Fixed SD Card is connected to the SDIO0 block in the PS using MIO pins 40-47.  I would like to connected a second SD Card using the PModSD from Digilent (mentioned above) directly to the SDIO1 block in the PS by plugging it into the MIO PMOD (JE1).   

    I have come to the conclusion that Digilent's PModSD is not compatible with the MIO PMOD (JE1).   Using JE1 and PModSD, the mappings  are fixed (SD-func <-> PMod pin# <-> MIO#) but incorrect.  For example, the SD-cmd is connected to PMod pin #2, which in turn connects to MIO_10.  The only SDIO1 pin which MIO_10 connects to is IO-Bit0, but the SD-cmd signal needs to be connected to Command pin, which is only accessible through MIO_11.  

    I feel that I might be missing something, since this use-case seems fairly obvious.  I I can see how I might connect the PModSD to the SDIO1 controller on the PS7 using EMIO and one of PMods connected to the PL.  The reason I want to avoid this is that I am already short on PMod connections to the PL...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • bhfletcher
    0 bhfletcher over 11 years ago in reply to e14 Contributor

    Seems you cross-posted this in 2 places. Please don't do that. An answer is provided under your other post under ZedBoard Forum.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • bhfletcher
    0 bhfletcher over 11 years ago in reply to e14 Contributor

    Seems you cross-posted this in 2 places. Please don't do that. An answer is provided under your other post under ZedBoard Forum.

    Bryan