Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Rewriting configuration SPI flash memory on MicroZED
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 731 views
  • Users 0 members are here
Related

Rewriting configuration SPI flash memory on MicroZED

e14 Contributor
e14 Contributor over 10 years ago

I have a  MicroZed 7020 eval board. 

1)  I would like to know if it is possible to reprogram the onboard configuration SPI flash using the ZYNQ processor.  I would like to transmit a BIT file over Ethernet to the ZYNQ processor and then have the processor write it to the SPI Flash memory to update the FPGA code.

On the MicroZED Rev F schematic, I noticed that the SPI flash control lines are connected to PS_MIO1, PS_MIO2, PS_MIO3, PS_MIO4, PS_MIO5, PS_MIO6.

2)   Can these same control lines be used for rewriting the SPI flash after the FPGA has configured? 
Or do these pins become tristated after configuration is complete?



3) Is there a dedicated hardware resource that handles the SPI configuration programming on bootup?

It is not clear to me whether this SPI configuration flash uses the embedded SPI0 or SPI1 hardware resources that is part of the ZYNQ.


I am using Vivado 2015.1  with project settings->general->project device->MicroZed 7020 Board (xc7z020clg400-1)

Thank you



  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hello Frank,

     

    You can write the the QSPI Flash on the MicroZed board after the FPGA has been configured. If you are using Linux you might want to take a look at this Xilinx Tech Tip that came up with a quick Google search:

     

    http://www.wiki.xilinx.com/Zynq-7000+AP+SoC+Boot+-+Programmable+Logic+Configuration+via+Ethernet+Tech+Tip

     

    This forum post might be useful as well:

     

    http://zedboard.org/content/how-flash-fsbl-only-qspi

     

    You can perform the same function in a 'bare metal' or standalone system. In that case I would suggest you look at the low level driver examples available in the SDK. Take a look at this forum post in that case:

     

    http://zedboard.org/content/writing-file-flash-memory-and-reading-it-pspl

     

     

    -Gary