Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Confusion in BKO and MicroZed HW User Guide
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 367 views
  • Users 0 members are here
Related

Confusion in BKO and MicroZed HW User Guide

e14 Contributor
e14 Contributor over 12 years ago

In the BKO Guide: http://zedboard.com/support/documentation/2182 (15.May.14)

Zynq AP SoC Pin Names index from one, where the MicroZed HW guide: http://zedboard.com/support/documentation/1519 (18.Jun.14)
index from zero.

eg.
On the BKO:
CON1, pin 19 --- JX1, pin 29 --- Bank 34, Y16 --- IO_L7P_T1_34
IS NOT!!
JX1_LVDS_7_P

it is actually JX1_LVDS_6_P


Though their naming conventions differ, is it safe to simply match JX1 Pin# and Zynq AP SoC Connection?

Thanks,
//Seather

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Sorry for the confusion. The net names are really 'apples' and 'oranges'. The JX1_LVDS_6_P listed in the MicroZed HW Users Guide is just a net name made up to indicate the LVDS pairs available. The IO_L7P_T1_34 net name used in the BKO Users Guide is the actual signal name from the Zynq device. Both refer to the Zynq pin Y16 in Bank 34, so yes it is OK.

     

    We will try to be more consistent in our naming conventions.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Sorry for the confusion. The net names are really 'apples' and 'oranges'. The JX1_LVDS_6_P listed in the MicroZed HW Users Guide is just a net name made up to indicate the LVDS pairs available. The IO_L7P_T1_34 net name used in the BKO Users Guide is the actual signal name from the Zynq device. Both refer to the Zynq pin Y16 in Bank 34, so yes it is OK.

     

    We will try to be more consistent in our naming conventions.

     

    -Gary