Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design How to flash FSBL only into QSPI?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 362 subscribers
  • Views 2391 views
  • Users 0 members are here
Related

How to flash FSBL only into QSPI?

e14 Contributor
e14 Contributor over 11 years ago

Hi all,
I successfully built a new FSBL for my MicroZed based on my hardware design.
Is it possible to flash it into QSPI, without touching the only u-boot?
On other Zynq boards I successfully did this with u-boot, by uploading the new FSBL binary from TFTP and writing it with "sf write" to address 0x40000 (but I do not know from where this address came from).
Or I have to rebuild also u-boot from source, rebuild a BOOT.BIN and flash it?

Thanks
Davide

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Davide,

    Yes, these instructions should be okay for MicroZed with a starting QSPI address of 0 as well.

    As for the correct filename, you are correct.

    The boot.mcs file is a special format that should be used with the Xilinx SDK "Program Flash" tool.

    If you are doing the QSPI write from U-boot, then the using the boot.bin container format is appropriate.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Davide,

    Yes, these instructions should be okay for MicroZed with a starting QSPI address of 0 as well.

    As for the correct filename, you are correct.

    The boot.mcs file is a special format that should be used with the Xilinx SDK "Program Flash" tool.

    If you are doing the QSPI write from U-boot, then the using the boot.bin container format is appropriate.

    Regards,

    -Kevin