Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Ethernet LEDs constant on and not blinking
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 6 replies
  • Subscribers 362 subscribers
  • Views 1168 views
  • Users 0 members are here
Related

Ethernet LEDs constant on and not blinking

e14 Contributor
e14 Contributor over 11 years ago

I seem to have the problem described in section 3.4 of http://zedboard.org/sites/default/files/documentations/MicroZed_RevBCF_Errata_140523a.pdf.  "Ethernet LEDs constant on and not blinking".  Once my Ethernet LEDs go on, they never go off (nor do they blink).

I have a Rev F board, but it must be one of these early ones.

The solution in the errata is to use MicroZed_Linux_sd_image_v1_1_131212.zip.  However, I want to use my own custom design.  How do I implement the fix in my design?  Where do I make the change?  Is there a hardware fix I should make?  Any guidance would be appreciated.

Thanks.

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi Jerry,

    Thanks for confirming that the change made a difference. 

    Further details on the operation of the LED modes is covered in the Marvell datasheet for the Ethernet PHY. 

    Do you have an Avnet/Silica FAE that you are working with?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi Jerry,

    Thanks for confirming that the change made a difference. 

    Further details on the operation of the LED modes is covered in the Marvell datasheet for the Ethernet PHY. 

    Do you have an Avnet/Silica FAE that you are working with?

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to zedhed

    Kevin,
    I'll ask my FAE for the Marvell datasheet.  It is certainly better now, but I would not say it is correct.  I don't get a green light, which I'm sure I should.  (As I said, it seems on but very dim...but I now think that it really is off, and the dim light is bleed over from the yellow.)  So I think the initialization or something isn't quite right and green just doesn't work, but at least the yellow is flashing, and I get no lights when there is no connection.  That is the most important since I lost a few hours battling a networking issue when I mistakenly thought I had a connection due to the lights being on.  Ugh!

    Jerry