Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Internal PL LED Access
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1262 views
  • Users 0 members are here
Related

Internal PL LED Access

walden95
walden95 over 9 years ago

I have a Microzed XC7010 board and am trying to access an available onboard LED for debug information for the PL side of the board.

From the schematics, it seems that the only appropriate LED is the Blue LED on the DONE_0 port of Bank 0. However, I'm not finding it easily accessible to the PL without having to go outside the board. How can I connect to this or any other LED to the PL?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Walden,

    That blue led is not accessible to you. If you wish to create a clock in the PL, you can enable a PL clock by double clicking on your Zynq Processor then going to the Clock configuration settings. When in the clock configuration settings you can enable/define the frequency of up to 4 PL clocks.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Walden,

    That blue led is not accessible to you. If you wish to create a clock in the PL, you can enable a PL clock by double clicking on your Zynq Processor then going to the Clock configuration settings. When in the clock configuration settings you can enable/define the frequency of up to 4 PL clocks.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • walden95
    0 walden95 over 9 years ago in reply to jafoste4

    Thanks JFoster,

    I'm moving onto something else at the moment, but I just want to make sure that we are on the same page regarding that Blue LED if I so choose to come back to it, or for anyone else curious. I've included the images that I was looking at in the schematic that made me think it was accessible.

     

    imageimage

    image

     

    I understand now that I can't access Bank 0 from the PL.

    However, I do not understand why it is not possible to control the Blue LED via the first microheader (JX1), even if that means I need to hook a wire or two (Probably GND through a tri-state-buffer) externally to the board. Is there some state whilst the board is on and programmed that pulls FPGA_DONE to GND (Turning off the Blue LED) that makes it unsuitable for use?

    Thanks for your responses.