Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Internal PL LED Access
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 363 subscribers
  • Views 1260 views
  • Users 0 members are here
Related

Internal PL LED Access

walden95
walden95 over 9 years ago

I have a Microzed XC7010 board and am trying to access an available onboard LED for debug information for the PL side of the board.

From the schematics, it seems that the only appropriate LED is the Blue LED on the DONE_0 port of Bank 0. However, I'm not finding it easily accessible to the PL without having to go outside the board. How can I connect to this or any other LED to the PL?

Thanks!

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 9 years ago

    Hello Walden,

    The Blue Done Led is not a user axxessible led. That Led is enumerated when the bitstream was sucessfully loaded into the pfga. The only user LED is a PS led (D3). Take a look at the hardware user guide section 2.6.2

    http://zedboard.org/support/documentation/1519

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • walden95
    0 walden95 over 9 years ago in reply to jafoste4

    Is there a way to connect that pin to something the PL can use?

    For the Blue LED, I would need a GND pin and the FPGA_DONE pin connected externally.

    For that Red LED, I would need a way to send a signal between the PS and PL since the PL does not have acess to Bank 501. Is there a block for this similar to creating a clock for the PL?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • walden95
    0 walden95 over 9 years ago in reply to jafoste4

    Is there a way to connect that pin to something the PL can use?

    For the Blue LED, I would need a GND pin and the FPGA_DONE pin connected externally.

    For that Red LED, I would need a way to send a signal between the PS and PL since the PL does not have acess to Bank 501. Is there a block for this similar to creating a clock for the PL?