Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Unable to open the file
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 1924 views
  • Users 0 members are here
Related

Unable to open the file

szeyong
szeyong over 9 years ago

Hi, we have faced some problems when we tried to open the files in vivado software. The hardware we are using is  ZYNQ XC72Z020 CLG400ABX1601 D5170858A

The error is stated below. 

 

ERROR: [Board 49-71] The board_part definition was not found for em.avnet.com:microzed_7020:part0:1.1. The project's board_part property was not set, but the project's part property was set to xc7z020clg400-1. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.

 

Any possible solution is appreciated. Thank You!

  • Sign in to reply
  • Cancel
Parents
  • szeyong
    0 szeyong over 9 years ago

    We tried to followed the instructions given. However, we are unable to open the folder

     

    cd D:/FYP_FPGA/AES-MBCC-EMBV-DEV-G_PYTHON1300C_HLS_2015_4_01/embv_hls_2015_4_01/embv_hls/embv/hardware/vivado

    source ./scripts/create_project.tcl

    # set project_dir "project"

    # set ip_dir "srcs/ip"

    # set hdl_dir "srcs/hdl"

    # set ui_dir "srcs/ui"

    # set constrs_dir "constrs"

    # set scripts_dir "scripts"

    # if { $argc > 1 } {

    #    puts "ERROR: Specify target platform: '-tclargs embv'

    #    exit

    # }

    # if { $argc == 0 || $argv eq "embv" } {

    #    set platform "embv"

    #    set part "xc7z020clg400-1"

    #    set board_part "em.avnet.com:microzed_7020:part0:1.1"

    # } else {

    #    puts "ERROR: Incorrect or unknown target platform selected: '$argv'"

    #    exit

    # }

    # puts "INFO: Target platform selected: '$platform'"

    INFO: Target platform selected: 'embv'

    # set design_name "embv_top"

    # set pin_xdc_file "pin_${platform}.xdc"

    # set timing_xdc_file "timing_${platform}.xdc"

    # set ps7_config_file "ps7_config_${platform}.tcl"

    # create_project $design_name $project_dir -part $part -force

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'D:/FYP_FPGA/AES-MBCC-EMBV-DEV-G_PYTHON1300C_HLS_2015_4_01/embv_hls_2015_4_01/embv_hls/embv/hardware/vivado/project'

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1704] No user IP repositories specified

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2016.4/data/ip'.

    # set_property board_part $board_part [current_project]

    ERROR: [Board 49-71] The board_part definition was not found for em.avnet.com:microzed_7020:part0:1.1. The project's board_part property was not set, but the project's part property was set to xc7z020clg400-1. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • szeyong
    0 szeyong over 9 years ago

    We tried to followed the instructions given. However, we are unable to open the folder

     

    cd D:/FYP_FPGA/AES-MBCC-EMBV-DEV-G_PYTHON1300C_HLS_2015_4_01/embv_hls_2015_4_01/embv_hls/embv/hardware/vivado

    source ./scripts/create_project.tcl

    # set project_dir "project"

    # set ip_dir "srcs/ip"

    # set hdl_dir "srcs/hdl"

    # set ui_dir "srcs/ui"

    # set constrs_dir "constrs"

    # set scripts_dir "scripts"

    # if { $argc > 1 } {

    #    puts "ERROR: Specify target platform: '-tclargs embv'

    #    exit

    # }

    # if { $argc == 0 || $argv eq "embv" } {

    #    set platform "embv"

    #    set part "xc7z020clg400-1"

    #    set board_part "em.avnet.com:microzed_7020:part0:1.1"

    # } else {

    #    puts "ERROR: Incorrect or unknown target platform selected: '$argv'"

    #    exit

    # }

    # puts "INFO: Target platform selected: '$platform'"

    INFO: Target platform selected: 'embv'

    # set design_name "embv_top"

    # set pin_xdc_file "pin_${platform}.xdc"

    # set timing_xdc_file "timing_${platform}.xdc"

    # set ps7_config_file "ps7_config_${platform}.tcl"

    # create_project $design_name $project_dir -part $part -force

    INFO: [ProjectBase 1-489] The host OS only allows 260 characters in a normal path. The project is stored in a path with more than 80 characters. If you experience issues with IP, Block Designs, or files not being found, please consider moving the project to a location with a shorter path. Alternately consider using the OS subst command to map part of the path to a drive letter.

    Current project path is 'D:/FYP_FPGA/AES-MBCC-EMBV-DEV-G_PYTHON1300C_HLS_2015_4_01/embv_hls_2015_4_01/embv_hls/embv/hardware/vivado/project'

    INFO: [IP_Flow 19-234] Refreshing IP repositories

    INFO: [IP_Flow 19-1704] No user IP repositories specified

    INFO: [IP_Flow 19-2313] Loaded Vivado IP repository 'C:/Xilinx/Vivado/2016.4/data/ip'.

    # set_property board_part $board_part [current_project]

    ERROR: [Board 49-71] The board_part definition was not found for em.avnet.com:microzed_7020:part0:1.1. The project's board_part property was not set, but the project's part property was set to xc7z020clg400-1. Valid board_part values can be retrieved with the 'get_board_parts' Tcl command. Check if board.repoPaths parameter is set and the board_part is installed from the tcl app store.