Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Constraint File Variable Definitions
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 421 views
  • Users 0 members are here
Related

Constraint File Variable Definitions

rrsquez
rrsquez over 9 years ago

Hello. The following is a line from the MicroZed constraint file (microzed_7z010_master_XDC_RevB_v1.xdc).

Here is one line:

set_property PACKAGE_PIN T10 [get_ports{JX1_LVDS_0_N}]

Where is definition for "JX1_LVDS_0_N" and the other variables used in these constraint files?

 

Another example:

The Zedboard also has a constraint file (zedboard_master_XDC_RevC_D_v3.xdc) that also uses variables in this manner.

Here is one line: 

set_property PACKAGE_PIN U11  [get_ports {OLED_VBAT}];  # "OLED-VBAT"

Again, where would the "OLED_VBAT" variable be defined? It is a number between 54 and 57.
 

Thank you, Richard V

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 9 years ago

    When pinning differential pairs in a constraint file, you only need to enter in the _P.  The _N will automatically come along for the ride!

    If you use those pins for SINGLE ended, you will need to modify the constraint.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rrsquez
    0 rrsquez over 9 years ago in reply to drozwood90

    Hello Dan. Sorry, but you still haven't answered my question.

    This is 1 line from the constraint file provided on the website:

    set_property PACKAGE_PIN T10 [get_ports{JX1_LVDS_0_N}

     

    Again, I have to ask:
    Where is definition for "JX1_LVDS_0_N" and the other constants used in these constraint files? I didn't create this file. I don't care that it's a differential signal.

     

    Thank you, Richard V

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • rrsquez
    0 rrsquez over 9 years ago in reply to drozwood90

    Hello Dan. Sorry, but you still haven't answered my question.

    This is 1 line from the constraint file provided on the website:

    set_property PACKAGE_PIN T10 [get_ports{JX1_LVDS_0_N}

     

    Again, I have to ask:
    Where is definition for "JX1_LVDS_0_N" and the other constants used in these constraint files? I didn't create this file. I don't care that it's a differential signal.

     

    Thank you, Richard V