Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design SW1 Glow RED when I connect USB cable
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 13 replies
  • Subscribers 361 subscribers
  • Views 1800 views
  • Users 0 members are here
Related

SW1 Glow RED when I connect USB cable

e14 Contributor
e14 Contributor over 11 years ago

I have seen this strange behavior with my zedboard, when I connect usb as power cable SW1 glows RED and D5-R41 Blue. This behavior is irrespective of boot_mode jumper settings JP1-JP3, I'm unable to boot the board.

Can anyone help?

  • Sign in to reply
  • Cancel
Parents
  • bhfletcher
    0 bhfletcher over 11 years ago

    The Platform Cable USB from Xilinx is supported with MicroZed. Are you using a supported operating system? If you are having trouble with the Xilinx tools and cable, you should contact Xilinx support.

    Bryan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    Finally I was able connect platform cable.

    I downloaded fsbl and u-boot but nothing comes up on uart can you see below setps.

    xsdb% connect                                                                                                                 
    tcfchan#0
    xsdb% targets                                                                                                                 
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsdb% targets 4                                                                                                               
    xsdb% fpga -f /opt/sys.bit                                                                                                    
    100%    1MB   0.4MB/s  00:05                                                                                                  
    xsdb% targets                                                                                                                 
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4* xc7z010
    xsdb% targets 2                                                                                                               
    xsdb% targets                                                                                                                 
      1  APU
         2* ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsdb% dow /opt/fsbl.elf                                                                                                       
    Downloading Program -- /opt/fsbl.elf                                                                                          
    tsection, .text: 0x00000000 - 0x0000f76f
    tsection, .handoff: 0x0000f770 - 0x0000f7bb
    tsection, .init: 0x0000f7bc - 0x0000f7d3
    tsection, .fini: 0x0000f7d4 - 0x0000f7eb
    tsection, .rodata: 0x0000f7ec - 0x00010ae3
    tsection, .data: 0x00010ae8 - 0x00013987
    tsection, .eh_frame: 0x00013988 - 0x0001398b
    tsection, .mmu_tbl: 0x00014000 - 0x00017fff
    tsection, .init_array: 0x00018000 - 0x00018007
    tsection, .fini_array: 0x00018008 - 0x0001800b
    tsection, .rsa_ac: 0x0001800c - 0x0001903f
    tsection, .bss: 0x00019040 - 0x0001ae4b
    tsection, .heap: 0x0001ae4c - 0x0001ce4f
    tsection, .stack: 0xffff0000 - 0xffffd3ff
    100%    0MB   0.1MB/s  00:01                                                                                                  
    Setting PC to Program Start Address 0x00000000
    Successfully downloaded /opt/fsbl.elf
    xsdb% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff28 (Suspended)
    xsdb% con                                                                                                                     
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running
    xsdb% stop                                                                                                                    
    xsdb% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xf790 (Suspended)                                                  
    xsdb% dow /opt/u-boot                                                                                                         
    Downloading Program -- /opt/u-boot
    tsection, .text: 0x04000000 - 0x0403b573
    tsection, .rodata: 0x0403b574 - 0x040499d2
    tsection, .hash: 0x040499d4 - 0x040499ff
    tsection, .dtb.init.rodata: 0x04049a00 - 0x0404ba0f
    tsection, .data: 0x0404ba10 - 0x0404de63
    tsection, .got.plt: 0x0404de64 - 0x0404de6f
    tsection, .u_boot_list: 0x0404de70 - 0x0404ea2b
    tsection, .rel.dyn: 0x0404ea2c - 0x04056dab
    tsection, .bss_start: 0x0404ea2c - 0x0404ea2b
    tsection, .bss: 0x0404ea2c - 0x0408ead7
    tsection, .bss_end: 0x0408ead8 - 0x0408ead7
    100%    0MB   0.1MB/s  00:05                                                                                                  
    Setting PC to Program Start Address 0x04000000
    Successfully downloaded /opt/u-boot
    xsdb% con                                                                                                                     
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running


    Was the steps executed fine? let me know if I missed anything?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to bhfletcher

    Finally I was able connect platform cable.

    I downloaded fsbl and u-boot but nothing comes up on uart can you see below setps.

    xsdb% connect                                                                                                                 
    tcfchan#0
    xsdb% targets                                                                                                                 
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsdb% targets 4                                                                                                               
    xsdb% fpga -f /opt/sys.bit                                                                                                    
    100%    1MB   0.4MB/s  00:05                                                                                                  
    xsdb% targets                                                                                                                 
      1  APU
         2  ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4* xc7z010
    xsdb% targets 2                                                                                                               
    xsdb% targets                                                                                                                 
      1  APU
         2* ARM Cortex-A9 MPCore #0 (Running)
         3  ARM Cortex-A9 MPCore #1 (Running)
      4  xc7z010
    xsdb% dow /opt/fsbl.elf                                                                                                       
    Downloading Program -- /opt/fsbl.elf                                                                                          
    tsection, .text: 0x00000000 - 0x0000f76f
    tsection, .handoff: 0x0000f770 - 0x0000f7bb
    tsection, .init: 0x0000f7bc - 0x0000f7d3
    tsection, .fini: 0x0000f7d4 - 0x0000f7eb
    tsection, .rodata: 0x0000f7ec - 0x00010ae3
    tsection, .data: 0x00010ae8 - 0x00013987
    tsection, .eh_frame: 0x00013988 - 0x0001398b
    tsection, .mmu_tbl: 0x00014000 - 0x00017fff
    tsection, .init_array: 0x00018000 - 0x00018007
    tsection, .fini_array: 0x00018008 - 0x0001800b
    tsection, .rsa_ac: 0x0001800c - 0x0001903f
    tsection, .bss: 0x00019040 - 0x0001ae4b
    tsection, .heap: 0x0001ae4c - 0x0001ce4f
    tsection, .stack: 0xffff0000 - 0xffffd3ff
    100%    0MB   0.1MB/s  00:01                                                                                                  
    Setting PC to Program Start Address 0x00000000
    Successfully downloaded /opt/fsbl.elf
    xsdb% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xffffff28 (Suspended)
    xsdb% con                                                                                                                     
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running
    xsdb% stop                                                                                                                    
    xsdb% Info: ARM Cortex-A9 MPCore #0 (target 2) Stopped at 0xf790 (Suspended)                                                  
    xsdb% dow /opt/u-boot                                                                                                         
    Downloading Program -- /opt/u-boot
    tsection, .text: 0x04000000 - 0x0403b573
    tsection, .rodata: 0x0403b574 - 0x040499d2
    tsection, .hash: 0x040499d4 - 0x040499ff
    tsection, .dtb.init.rodata: 0x04049a00 - 0x0404ba0f
    tsection, .data: 0x0404ba10 - 0x0404de63
    tsection, .got.plt: 0x0404de64 - 0x0404de6f
    tsection, .u_boot_list: 0x0404de70 - 0x0404ea2b
    tsection, .rel.dyn: 0x0404ea2c - 0x04056dab
    tsection, .bss_start: 0x0404ea2c - 0x0404ea2b
    tsection, .bss: 0x0404ea2c - 0x0408ead7
    tsection, .bss_end: 0x0408ead8 - 0x0408ead7
    100%    0MB   0.1MB/s  00:05                                                                                                  
    Setting PC to Program Start Address 0x04000000
    Successfully downloaded /opt/u-boot
    xsdb% con                                                                                                                     
    Info: ARM Cortex-A9 MPCore #0 (target 2) Running


    Was the steps executed fine? let me know if I missed anything?