Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Setting MAC ID
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 689 views
  • Users 0 members are here
Related

Setting MAC ID

e14 Contributor
e14 Contributor over 11 years ago

I have two microZeds and need them to have unique MAC addresses.  I've try to set the MAC address in UBOOT via "setenv ethaddr 00:0a:35:XX:YY:ZZ" but when Linux boots, it seems to still have the default address of 00:0a:35:00:01:22 and a reboot shows UBOOT is back to the default.  In UBOOT I do a "printenv ethaddr" and can see I changed the value.

I have a microZed FMC carrier, and found that in section 2.1.1 of the User Guide it says there is a MAC ID EEPROM, but the info there is too sparce for me to figure out how to use it and have Linux read it.

What I don't understand is that I would have thought this would be in the QSPI, and that changing it in UBOOT would update the QSPI, and that Linux would read it from the QSPI.  Does this mean I have a problem with the devicetree?

Can anyone provide guidance here?  Thanks!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Looks like I just needed another reboot.  It now works.

    So, I consider there to be a bug in UBOOT for the microZed.  Specifically, I recommend the following change:

         u-boot-xlnx/include/configs/zynq_microzed.h

    add

         #define CONFIG_ZYNQ_QSPI

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Looks like I just needed another reboot.  It now works.

    So, I consider there to be a bug in UBOOT for the microZed.  Specifically, I recommend the following change:

         u-boot-xlnx/include/configs/zynq_microzed.h

    add

         #define CONFIG_ZYNQ_QSPI