Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Python 1300-C Camera Module interface to HP Banks
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 363 subscribers
  • Views 1661 views
  • Users 0 members are here
Related

Python 1300-C Camera Module interface to HP Banks

e14 Contributor
e14 Contributor over 11 years ago

Hello,

I would like to use the Python 1300-C Camera module for my Xilinx VC707 evaluation kit. Unfortunatey, the camera hardware user guide says to connect the 2.5V LVDS signals to Xilinx HR banks. My Virtex-7 only has 1.8V HP banks. Despite the voltage difference, I know it is still theoretically possible by using external terminating resistors.

My question is if anyone tried attaching this camera to non zedboards? Does the external terminators degrade the signal since it is now so far away from the receiver? What was your experience like? Also...why is it so hard to get this sensor's extensive datasheet? Seems a little bit weird to keep it such a secret.

Any kind of discussion on this matter would be incredibly helpful.

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • albertabeef
    0 albertabeef over 11 years ago

    The short answer to your question, yes the PYTHON-1300-C is supported by 1.8V HP I/O Banks.

    The receiver for the PYTHON-1300-C image sensor uses LVDS signaling with LVDS differential termination (DIFF_TERM = 'TRUE')

    The  differential termination is available in two configurations:

    - 2.5V HR I/O Banks, using the LVDS_25 I/O standard and DIFF_TERM set to 'TRUE'

    - 1.8V HP I/O Banks, using the LVDS I/O standard and DIFF_TERM set to 'TRUE'

    Here is a Xilinx reference that provides a good detailed description on these two supported configurations:

       http://www.xilinx.com/support/answers/43989.html

     

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • albertabeef
    0 albertabeef over 11 years ago

    The short answer to your question, yes the PYTHON-1300-C is supported by 1.8V HP I/O Banks.

    The receiver for the PYTHON-1300-C image sensor uses LVDS signaling with LVDS differential termination (DIFF_TERM = 'TRUE')

    The  differential termination is available in two configurations:

    - 2.5V HR I/O Banks, using the LVDS_25 I/O standard and DIFF_TERM set to 'TRUE'

    - 1.8V HP I/O Banks, using the LVDS I/O standard and DIFF_TERM set to 'TRUE'

    Here is a Xilinx reference that provides a good detailed description on these two supported configurations:

       http://www.xilinx.com/support/answers/43989.html

     

    Regards,

    Mario.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer