Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design program microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 399 views
  • Users 0 members are here
Related

program microzed

e14 Contributor
e14 Contributor over 11 years ago

is the only way to program/configure bit/elf file for microzed is using the usb-uart?  No jtag?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    As detailed in the MicroZed Hardware Users Guide available for download here: http://zedboard.org/support/documentation/1519 an external JTAG cable is required.

     

    2.9.1 JTAG MicroZed requires an external JTAG cable for JTAG operations. MicroZed is designed with the Platform Cable JTAG connector, Molex 87832-1420 which is a 2.0mm 2x7 shrouded, polarized header. On MicroZed, this is J3 and is compatible with Xilinx Platform Cables and Digilent JTAG HS1 or HS2 Programming Cables. The JTAG Reset signal is connected to PS_SRST_B through an open-drain buffer.

     

    The new Digilent HS3 JTAG Programming Cable works as well.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    As detailed in the MicroZed Hardware Users Guide available for download here: http://zedboard.org/support/documentation/1519 an external JTAG cable is required.

     

    2.9.1 JTAG MicroZed requires an external JTAG cable for JTAG operations. MicroZed is designed with the Platform Cable JTAG connector, Molex 87832-1420 which is a 2.0mm 2x7 shrouded, polarized header. On MicroZed, this is J3 and is compatible with Xilinx Platform Cables and Digilent JTAG HS1 or HS2 Programming Cables. The JTAG Reset signal is connected to PS_SRST_B through an open-drain buffer.

     

    The new Digilent HS3 JTAG Programming Cable works as well.

     

    -Gary