Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Deadlock of Microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 361 subscribers
  • Views 1643 views
  • Users 0 members are here
Related

Deadlock of Microzed

e14 Contributor
e14 Contributor over 10 years ago

Hello

I work with Vivado 2014.2 and the AES-Z7MB-7Z020-SOM-I-G.

Iu2019m new to the Zynq world and worked through the ZynqSW and ZynqHW tutorials for the Zedboard (we already had Zedboards) as well as the CTT tutorial. Then I wanted to adapt the CTT tutorial to my target hardware, the Microzed (version with a Z7020).

Since it is a lot of new stuff that is discussed, it happened that I corrupted my Microzed somehow. I managed to crash my serial console, the zynq just doesnu2019t send any message (Tx of Zynq is always 1V8) even though Iu2019m able to download some (default) helloworld projects or connect to the zynq via XMD console.
However, I was able to debug the helloworld.c file andu2026 see there. I have the same deadlock as described here:

https://lists.rtems.org/pipermail/users/2015-May/028793.html


My Debug Disassembly exctract is this:
ffffff2c:   dsb     sy
ffffff30:   wfe
ffffff34:   mvn     r0, #15
ffffff38:   ldr     lr, [r0]
ffffff3c:   cmn     lr, #212
ffffff40:   beq     -28     ; addr=0xffffff2c

This exact same disassembly extract appears with any code I try to debug on the microzed now.

Can you tell me if there is a way to overcome this deadlock? Is there a way to download an fsbl and bring the PS up and running again?

I would be very happy for an answer or even a way to reset my system again.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary

    I compared a design run for a Microzed (MZ) 7010 and 7020 today where I did exactly the same for one board and then for the other. With the result that on MZ 7010 I successfully download and even debug the helloworld program. On MZ 7020 I can successfully download the program without any results on serial terminal. When I try to debug on MZ 7020 it doesn't start at the beginning of main (as it does on MZ 7010 or Zedboard).

    I proceeded as follows for MZ 7010 and MZ 7020:
    1) create new project with vivado2014.2 with MZ_70x0 as project device
    2) in block design: processing_system7_0 settings: preset Microzed
    3) Block Automation, create HDL wrapper, create bitstream
    4) export hardware (with bitstream), launch SDK
    5) create Hello World app project (with bsp and default Hello World template)
    6) power MZ, start TeraTerm (with correct settings)
    7a) download Hello World (reset entire system and prog. FPGA)
    7b) debug Hello World (dito)

    Comparing the results I must conclude that either the MicroZed Board Definition files for MZ 7020 or my MZ 7020 is corrupted. Or do you have another conlusion? Can you send me an RMA for my MZ 7020 or support me in another way?

    Regards
    Nicolas

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Hi Gary

    I compared a design run for a Microzed (MZ) 7010 and 7020 today where I did exactly the same for one board and then for the other. With the result that on MZ 7010 I successfully download and even debug the helloworld program. On MZ 7020 I can successfully download the program without any results on serial terminal. When I try to debug on MZ 7020 it doesn't start at the beginning of main (as it does on MZ 7010 or Zedboard).

    I proceeded as follows for MZ 7010 and MZ 7020:
    1) create new project with vivado2014.2 with MZ_70x0 as project device
    2) in block design: processing_system7_0 settings: preset Microzed
    3) Block Automation, create HDL wrapper, create bitstream
    4) export hardware (with bitstream), launch SDK
    5) create Hello World app project (with bsp and default Hello World template)
    6) power MZ, start TeraTerm (with correct settings)
    7a) download Hello World (reset entire system and prog. FPGA)
    7b) debug Hello World (dito)

    Comparing the results I must conclude that either the MicroZed Board Definition files for MZ 7020 or my MZ 7020 is corrupted. Or do you have another conlusion? Can you send me an RMA for my MZ 7020 or support me in another way?

    Regards
    Nicolas