Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design USB 0 hardware setup
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 362 subscribers
  • Views 1076 views
  • Users 0 members are here
Related

USB 0 hardware setup

smvo555
smvo555 over 12 years ago

Hi,

What is the proper way to connect bank 501 USB MIO pins to my design?
I want to set up communication between PC and Microzed.
Is it as easy to use as the USB UART which connects to the micro USB?

I'm not able to synchronize the read port of my dual port BRAM with the default USB UART connecting to the micro USB as there are no synchronization signals that I am aware of.

Thanks, advice is much appreciated

Sam

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The Zynq MIO pins associated with USB0 are connected directly to the SMSC USB3320 USB UART device on the MicroZed and are not available for connections.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • smvo555
    0 smvo555 over 12 years ago in reply to e14 Contributor

    Thank you for the reply,

    Looking at the schematic I see that the MSC USB3320 USB UART connects to the USB-A connector.
    Can I use the USB0 =>MSC USB3320 USB UART=>USB-A as my main data output from the system?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • smvo555
    0 smvo555 over 12 years ago in reply to e14 Contributor

    Thank you for the reply,

    Looking at the schematic I see that the MSC USB3320 USB UART connects to the USB-A connector.
    Can I use the USB0 =>MSC USB3320 USB UART=>USB-A as my main data output from the system?