Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed: Booting SD card for standalone case
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 362 subscribers
  • Views 1011 views
  • Users 0 members are here
Related

Microzed: Booting SD card for standalone case

100priya
100priya over 8 years ago
 
  

Hello,

  


    I am using Microzed board and i m stuck as i can't program it with SD card. I m using windows 8  and need help for bare-metal application.

  

I designed a simple 8-bit adder IP in Xilinx Vivado Design suite and used Zynq processor for providing clock.  I generated bitstream and launched SDK, generated FSBL application and then created an application to provide input to IP and to print the result (adder_output) of the adder IP on console.

  

I created boot image and copied the BOOT.bin file to SD card. I inserted the SD card into Microzed board and then connected the MicroZed board as well as Carrier card to the Laptop through USB-UART cable for both. 

  

But the blue LED won't glow and there is no output on the console.

  

Earlier, I just used Zynq processor to create "hello world" application. The LED glowed and i could see output on the console. But it is not working for IP cores.

  

Am i supposed to copy any other files on SD card in addition to boot.bin? Kindly suggest if i m missing something.

  

 

  

Thanks in advance!

  

Priya

 
  • Sign in to reply
  • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Priya,

    No, a boot.bin file should be all you need for baremetal SD Card boot.

    Does your application work when you load it over JTAG?

    What memory region is your application in? I know for instance the default configurations for the memory test application does not work via SD boot due to a conflict in memory region when booted via SD card.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100priya
    0 100priya over 8 years ago in reply to jafoste4

    Hi Josh,

     

    Thanx for replying. I don't have a Jtag cable. However, I tested it on Zedboard and it worked just fine.

    Could you plz tell me how do I check which memory region my application is in?

     

    --Priya

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • 100priya
    0 100priya over 8 years ago

    I m working on another project which has IP cores only on PL side. I/P and O/P communications are through PMOD/FMC pins. So I have nothing to write in the application in SDK. How do i create boot.bin in that case?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Priya,

    Refer to this post for your 2nd question https://forums.xilinx.com/t5/Embedded-Processor-System-Design/How-can-I-build-a-mcs-file-to-boot-the-PL-on-a-Zynq-from-SPI/td-p/499496

    You can check your memory section by looking at the linker scritp in you application (withing SDK)

    --Josh