Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed Petalinux 2016.1 BSP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 364 subscribers
  • Views 1238 views
  • Users 0 members are here
Related

Microzed Petalinux 2016.1 BSP

ghalady
ghalady over 10 years ago

I could not find BSPs for Microzed7010 for either Petalinux 2015.3 / 2015.4 or even 2016.1.  Has work stopped on Microzed now. I still wanted to work on these boards but am stranded without Petalinux BSP, also I couldn't get Microzed 2015.2 BSP to install with Petalinux 2015.2.1. I get the usage menu when I try doing "petalinux-create -t project -s <Directory_containing_Avnet_Microzed_7z010_2015_2_1_BSP_extract>

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Ghalady,

      I cannot see anything wrong with what you are doing, and I can follow the exact sequence you provided on my Linux host and it works perfectly.  So the only thing I can think of is that somehow your PetaLinux 2015.2.1 installation is corrupt.

    The only evidence I have (besides that your correct commands don't work) is that when I purposely enter an invalid bsp file name, I get back:

    realpath:  No such file or directory

    Error:  source mz_7020_2015_2_11.bsp doesn't exist!

    This is correct, because of the extra 1 in the name.  I notice in your installation, it returns the a specific line in the petalinux-create command, which is different than I see.  

    So my guess is that you should delete your 2015.2.1 PetaLinux installation, download a fresh version of the installer from the Xilinx site, make sure you validate the download by verifying the checksum, and reinstall.   Then give it another try.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago

    Ghalady,

      I cannot see anything wrong with what you are doing, and I can follow the exact sequence you provided on my Linux host and it works perfectly.  So the only thing I can think of is that somehow your PetaLinux 2015.2.1 installation is corrupt.

    The only evidence I have (besides that your correct commands don't work) is that when I purposely enter an invalid bsp file name, I get back:

    realpath:  No such file or directory

    Error:  source mz_7020_2015_2_11.bsp doesn't exist!

    This is correct, because of the extra 1 in the name.  I notice in your installation, it returns the a specific line in the petalinux-create command, which is different than I see.  

    So my guess is that you should delete your 2015.2.1 PetaLinux installation, download a fresh version of the installer from the Xilinx site, make sure you validate the download by verifying the checksum, and reinstall.   Then give it another try.

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to e14 Contributor

    I had the same issue and figured it out. The realpath utility included with that version of Petalinux does not work correctly. I installed a version of realpath from Ubuntu sudo apt-get install realpath and then replaced the version supplied with Petalinux with a link to /usr/bin/realpath. Everything worked after that.