Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed Petalinux 2016.1 BSP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 364 subscribers
  • Views 1238 views
  • Users 0 members are here
Related

Microzed Petalinux 2016.1 BSP

ghalady
ghalady over 10 years ago

I could not find BSPs for Microzed7010 for either Petalinux 2015.3 / 2015.4 or even 2016.1.  Has work stopped on Microzed now. I still wanted to work on these boards but am stranded without Petalinux BSP, also I couldn't get Microzed 2015.2 BSP to install with Petalinux 2015.2.1. I get the usage menu when I try doing "petalinux-create -t project -s <Directory_containing_Avnet_Microzed_7z010_2015_2_1_BSP_extract>

  • Sign in to reply
  • Cancel
Parents
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    The newer BSPs are intended to be automated in the build process.  The process and scripting needed for this does not look like it was released as of this posting.

    You can check back at the below page when the update is released publicly.
    http://microzed.org/support/design/1519/10

    As for building a newer released, the process should be the same flow - substituting the newer Petalinux files.  Please note that We have not worked through this flow as of this post so you are free to attempt that build yourself.  Once that has been released expect the post to be at the above link.  As I understand it, the newer build will be with the automated process, which means this will be slightly delayed due to this being the initial release.

    --Dan

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • drozwood90
    0 drozwood90 over 10 years ago

    Hi there,

    The newer BSPs are intended to be automated in the build process.  The process and scripting needed for this does not look like it was released as of this posting.

    You can check back at the below page when the update is released publicly.
    http://microzed.org/support/design/1519/10

    As for building a newer released, the process should be the same flow - substituting the newer Petalinux files.  Please note that We have not worked through this flow as of this post so you are free to attempt that build yourself.  Once that has been released expect the post to be at the above link.  As I understand it, the newer build will be with the automated process, which means this will be slightly delayed due to this being the initial release.

    --Dan