Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed breakout carrier card VCCIO pin level
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 7 replies
  • Subscribers 362 subscribers
  • Views 1176 views
  • Users 0 members are here
Related

Microzed breakout carrier card VCCIO pin level

100priya
100priya over 8 years ago

Hi,

 

There is a doubt I have ever since I started working on the microzed and breakout carrier card.

 

There is a VCCIO jumper on the carrier card which provides 3 options: 1.8V, 2.5V and 3.3V.  The following pins on carrier card are supposed to give out a voltage level (DC signal) as selected by the VCCIO jumper:

 

CON1: 53,54

CON2: 49,50

 

In order to check that the carrier card along with the VCCIO jumper are working fine, we should check the level of the above mentioned pins.

 

Well in my case, the above mentioned pins have a voltage level of 0.6V when I set the jumper to 1.8V position. These pins maintain the same voltage level even when I switch the jumper to 2.5V or 3.3V. Could anyone please suggest what might be the issue here? I feel that the carrier card has some problem. Should I get a new carrier card?

I am facing serious issues as all the output signals from CON1 and CON2 pins which are controlled by the VCCIO jumper are attenuated to below 0.5V.  Please suggest if I should buy a new card.

 

Thank you

Regards,

Priya Joshi

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Priya,

    I will confirm this tomorrow, I see what you are refering to in the schematic.

    In the mean time please measure VCCIO via the C4 Capacitor on the BKO and see if you are seeing the sellected VCCIO value.

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello Priya,

    I will confirm this tomorrow, I see what you are refering to in the schematic.

    In the mean time please measure VCCIO via the C4 Capacitor on the BKO and see if you are seeing the sellected VCCIO value.

    --Josh