Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design GPIO state at boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 821 views
  • Users 0 members are here
Related

GPIO state at boot

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I had a question regarding the GPIO status while powering on microZed, or any Zynq devices. It is state in the datasheet that MIO pins are tristate when applied power. But based on my logic analyzer, they are individually pulled up. I had also disabled the "pull up" during PS MIO configuration in Vivado.

https://dl.dropboxusercontent.com/u/83845564/GPIO.png

I'm planning to use some of the GPIO pins for the DC-DC power enable pin in an image sensor. Thus it is imperative all these MIO pins remain low until my program turns it on otherwise.

Could someone shed light on this? Or I have to use the IO on the logic side?

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Connecting a logic analyzer probe to a tristated signal, with no pull up or pull down, is not going to provide a valid result. By definition the signal is neither high nor low state.

     

    You will need to provide a pull down, either by external resistor or by enabling the internal pull down in the PS MIO configuration, to get the behavior you are looking for.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Connecting a logic analyzer probe to a tristated signal, with no pull up or pull down, is not going to provide a valid result. By definition the signal is neither high nor low state.

     

    You will need to provide a pull down, either by external resistor or by enabling the internal pull down in the PS MIO configuration, to get the behavior you are looking for.

     

    -Gary