Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design GPIO state at boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 821 views
  • Users 0 members are here
Related

GPIO state at boot

e14 Contributor
e14 Contributor over 11 years ago

Hi,

I had a question regarding the GPIO status while powering on microZed, or any Zynq devices. It is state in the datasheet that MIO pins are tristate when applied power. But based on my logic analyzer, they are individually pulled up. I had also disabled the "pull up" during PS MIO configuration in Vivado.

https://dl.dropboxusercontent.com/u/83845564/GPIO.png

I'm planning to use some of the GPIO pins for the DC-DC power enable pin in an image sensor. Thus it is imperative all these MIO pins remain low until my program turns it on otherwise.

Could someone shed light on this? Or I have to use the IO on the logic side?

Thanks in advance!

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks!

    I didn't realized the Saleae Logic default HiZ to 1 instead of 0. The voltage measurement on a pin is 0V and pulling down with 10k resistor shows expected behavior on the SPI controller.

    In the end, the logic inject 2.5V to the HiZ end. I guess this was to intended to avoid some unexpected behavior you just mentioned.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks!

    I didn't realized the Saleae Logic default HiZ to 1 instead of 0. The voltage measurement on a pin is 0V and pulling down with 10k resistor shows expected behavior on the SPI controller.

    In the end, the logic inject 2.5V to the HiZ end. I guess this was to intended to avoid some unexpected behavior you just mentioned.