Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Finicky GPIO on MIO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 1551 views
  • Users 0 members are here
Related

Finicky GPIO on MIO

e14 Contributor
e14 Contributor over 11 years ago

I am seeing strange behavior when I try to toggle a GPIO output on a MIO pin. The pin will toggle while in a debug session, but when the Zynq is configured by QSPI flash there is no pin response. The flash was programmed both by Impact and also through the SDK with the same result.

I configured the GPIO over MIO through Vivado and am using this blog post as a guide: http://forums.xilinx.com/t5/Xcell-Daily-Blog/Driving-the-Zynq-SoC-s-GPIO-Adam-Taylor-s-MicroZed-Chronicles/ba-p/389611

I am using MIO pin 12.

Any ideas?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    There is no obvious reason I can think of as to why GPIO would work in a debug session and not running when loaded from QSPI Flash.

     

    I would suggest first making sure that you have really successfully programmed you program into the QSPI Flash, perhaps using a 'Print' function to give an indication on the terminal that the program is actually running.

     

    The other difference may be one of timing. The nature of a debug session is that you can single step and even 'running' is slower. Perhaps add some delay in your program after toggling the pin to make sure you can observe the signal.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    There is no obvious reason I can think of as to why GPIO would work in a debug session and not running when loaded from QSPI Flash.

     

    I would suggest first making sure that you have really successfully programmed you program into the QSPI Flash, perhaps using a 'Print' function to give an indication on the terminal that the program is actually running.

     

    The other difference may be one of timing. The nature of a debug session is that you can single step and even 'running' is slower. Perhaps add some delay in your program after toggling the pin to make sure you can observe the signal.

     

    -Gary