Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Finicky GPIO on MIO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 1551 views
  • Users 0 members are here
Related

Finicky GPIO on MIO

e14 Contributor
e14 Contributor over 11 years ago

I am seeing strange behavior when I try to toggle a GPIO output on a MIO pin. The pin will toggle while in a debug session, but when the Zynq is configured by QSPI flash there is no pin response. The flash was programmed both by Impact and also through the SDK with the same result.

I configured the GPIO over MIO through Vivado and am using this blog post as a guide: http://forums.xilinx.com/t5/Xcell-Daily-Blog/Driving-the-Zynq-SoC-s-GPIO-Adam-Taylor-s-MicroZed-Chronicles/ba-p/389611

I am using MIO pin 12.

Any ideas?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks, Gary.

    I am adding the GPIO to an existing application with Ethernet. I have interrogated the board through a test app to confirm the rest of the program is running correctly after being configured by the flash.

    I will play with the timing and report back.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Thanks, Gary.

    I am adding the GPIO to an existing application with Ethernet. I have interrogated the board through a test app to confirm the rest of the program is running correctly after being configured by the flash.

    I will play with the timing and report back.