Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Finicky GPIO on MIO
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 362 subscribers
  • Views 1551 views
  • Users 0 members are here
Related

Finicky GPIO on MIO

e14 Contributor
e14 Contributor over 11 years ago

I am seeing strange behavior when I try to toggle a GPIO output on a MIO pin. The pin will toggle while in a debug session, but when the Zynq is configured by QSPI flash there is no pin response. The flash was programmed both by Impact and also through the SDK with the same result.

I configured the GPIO over MIO through Vivado and am using this blog post as a guide: http://forums.xilinx.com/t5/Xcell-Daily-Blog/Driving-the-Zynq-SoC-s-GPIO-Adam-Taylor-s-MicroZed-Chronicles/ba-p/389611

I am using MIO pin 12.

Any ideas?

  • Sign in to reply
  • Cancel
Parents
  • zedhed
    0 zedhed over 11 years ago

    Hi cobra18t,

    I have seen similar problems (but different than GPIO) with behavior when booting from flash that differ from the behavior when debugging.

    In each case, I was able to trace it back to my FSBL code (which is used to build the flash boot.mcs image file) was not updated with my new PS configuration.

    Since SDK uses the ps7_init.tcl file to initialize your Processing System each time a debug session is launched, perhaps this is also the case for you?

    Perhaps this is not the case for you, but it would be worth while to double check and make sure that you are using an FSBL which contains the ps7_init.c/ps7_init.h files that configure the MIO for the GPIO mode that you are trying to use.

    Regards,

    -Kevin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • zedhed
    0 zedhed over 11 years ago

    Hi cobra18t,

    I have seen similar problems (but different than GPIO) with behavior when booting from flash that differ from the behavior when debugging.

    In each case, I was able to trace it back to my FSBL code (which is used to build the flash boot.mcs image file) was not updated with my new PS configuration.

    Since SDK uses the ps7_init.tcl file to initialize your Processing System each time a debug session is launched, perhaps this is also the case for you?

    Perhaps this is not the case for you, but it would be worth while to double check and make sure that you are using an FSBL which contains the ps7_init.c/ps7_init.h files that configure the MIO for the GPIO mode that you are trying to use.

    Regards,

    -Kevin