Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Microzed 7010 Petalinux 2014.4 BSP
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 706 views
  • Users 0 members are here
Related

Microzed 7010 Petalinux 2014.4 BSP

ghalady
ghalady over 11 years ago

Though the VIVADO / SDK 2014.4 is out, I was not able to find the corresponding BSPs for Microzed 7010 board. Please provide pointers to the BSPs.

Thanks
Girish

  • Sign in to reply
  • Cancel
  • y_okada
    0 y_okada over 11 years ago

    This question is not replied at all. I am not sure whether zedboard.org is trying to prepare the BSP for 2014.4.

    Instead, I found BSP for 2014.4 for Zedboard at xilinx.
    http://www.xilinx.com/support/download/index.html/content/xilinx/en/downloadNav/petalinux.html

    I do not know the difference between those in xilinx and that in microzed.org.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Hi,

    I have also been looking for a 2014.4 BSP for the microzed board but only the zedboard is available.

    Why is the 2014.4 BSP not available?

    Is the 2014.4 zedboard BSP fully compatible with microzed?

    Can we use the microzed 2014.2 BSP with 2014.4 software?

    Regards,
    Eddy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Does microzed 2014.2 BSP work with 2014.4 Petalinux?  The Petalinux build problems with 2014.2 were corrected. In Petalinux 2014.4 a INITRAMRF Root filesystem works.  When using a JFFS2 root filesystem, no MTD devices are created.  What is missing?

    jasonbiggs@basler.com

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Petalinux 2014.2 with MicroZed BSP 2014.2 has QSPI Flash errors when using a JFFS@ Root filesystem type.  System works fine when Root filesystem type is INITRAMFS with combined image.ub (FIT image) but gives QSPI flash errors when booting Linux.  Linux version 3.14.2-xilinx
    jffs2: notice: (1) check_node_data: wrong data CRC in data node at 0x?????: read 0x?????, calculated 0x????.
    Kernel panic - not syncing: No working init found.  Try passing init= option to kernel. See Linux Documentation/init.txt for guidance.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The MicroZed 7010 and 7020 PetaLinux BSP for 2014.4 are now posted.

     

    Sorry for the delay, I made an error when I originally posted them.

     

    -Gary