Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design What is the Cost-Optimized C01 MicroZed SOM?
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 360 subscribers
  • Views 130 views
  • Users 0 members are here
Related

What is the Cost-Optimized C01 MicroZed SOM?

bhfletcher
bhfletcher over 11 years ago

The MicroZed User Guide was updated to v1.6 to add a bit more detail. Here are a couple table excerpts from the UG that explains the differences, complete with part numbers.

The UG goes on to explain that the MODE jumpers are removed from the Cost-Optimized (or C01) SOM and replaced with resistor jumpers that hard-wire the boot mode to QSPI. A different resistor mode setting may be requested from customize@avnet.com.

The main objective of the C01 is for volume production purchases where the cost savings is most important. You can see the cost savings and availability by searching at www.avnetexpress.com for "z7mb-7z010-C01" or "z7mb-7z020-C01"

Bryan

                                                                                                                                                                                                                               
   

Name

  
   

Part Number

  
   

Zynq Device

  
   

Tested Temperature Range

  
   

Evaluation Kit

  
   

AES-Z7MB-7Z010-G

  
   

XC7Z010-1CLG400C

  
   

0° to 70° C

  
   

7010 SOM

  
   

AES-Z7MB-7Z010-SOM-G

  
   

XC7Z010-1CLG400C

  
   

0° to 70° C

  
   

7010 Industrial SOM

  
   

AES-Z7MB-7Z010-SOM-I-G

  
   

XC7Z010-1CLG400I

  
   

-40° to 85° C*

  
   

7010 Cost-Optimized SOM

  
   

AES-Z7MB-7Z010-C01-G

  
   

XC7Z010-1CLG400C

  
   

0° to 70° C

  
   

7010 Industrial Cost-Optimized SOM

  
   

AES-Z7MB-7Z010-C01-I-G

  
   

XC7Z010-1CLG400I

  
   

-40° to 85° C*

  
   

7020 SOM

  
   

AES-Z7MB-7Z020-SOM-G

  
   

XC7Z020-1CLG400C

  
   

0° to 70° C

  
   

7020 Industrial SOM

  
   

AES-Z7MB-7Z020-SOM-I-G

  
   

XC7Z020-1CLG400I

  
   

-40° to 85° C*

  
   

7020 Cost-Optimized SOM

  
   

AES-Z7MB-7Z020-C01-G

  
   

XC7Z020-1CLG400C

  
   

0° to 70° C

  
   

7020 Industrial Cost-Optimized SOM

  
   

AES-Z7MB-7Z020-C01-I-G

  
   

XC7Z020-1CLG400I

  
   

-40° to 85° C*

  
 
 
                                                                                                                    
    

Name

   
    

Definition

   
    

Evaluation Kit

   
    

The evaluation kit version of MicroZed includes the Zynq 7010 device as well as several other items to make out-of-box evaluation simpler. These extra items include a micro-USB cable, Vivado Design Edition license voucher (device-locked to the 7010), 4 GB microSD card pre-loaded with a Linux test system, and a plastic carrying box. The majority of the tutorials published at www.microzed.org are targeted at this kit. The board included in the kit will work either as a standalone board or as a SOM plugged onto a carrier card.

   
    

SOM

   
    

System-on-module. These cards will work standalone or plugged into a carrier card. The SOM versions exclude a few items outlined in the Evaluation Kit definition above. The SOMs are intended to be sold in volume, for use with carrier cards.

   
    

Industrial SOM

   
    

Same as the SOM, except populated entirely with components that comply with a tested temperature range of -40° to 85° C, with the exception of the microSD card connector (502570-0893) which is rated at -25° to 85° C. Avnet has tested the Industrial SOMs to this temperature range with a thorough functional test. However, Avnet does not guarantee that the industrial SOM will function to this full temperature range under all conditions. End users are still responsible for proper airflow and heat mitigation.

   
    

Cost-Optimized SOM

   
    

This is identical to the SOM with the exception that all of the circuitry required for operating in standalone mode has been removed. The cost-optimized SOMs will ONLY work when plugged into a carrier card. The reduction in components allows these boards to be offered at a lower cost in volume. For a full listing of differences, see the yellow-highlighted items in the cost-optimized bill of materials.

   
    

Industrial Cost-Optimized SOM

   
    

Same as the Cost-Optimized SOM, except populated entirely with components that comply with a tested temperature range of -40° to 85° C, with the exception of the microSD card connector (502570-0893) which is rated at -25° to 85° C. Avnet has tested the Industrial SOMs to this temperature range with a thorough functional test. However, Avnet does not guarantee that the industrial Cost-Optimized SOM will function to this full temperature range under all conditions. End users are still responsible for proper airflow and heat mitigation.