Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Input to XADC with BKO Card
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Subscribers 362 subscribers
  • Views 1170 views
  • Users 0 members are here
Related

Input to XADC with BKO Card

trillian
trillian over 8 years ago

Hi there,

I have a MicroZed 7020 Board and want to read VN/VP values. Vor my IO Ports Vivado lets me only choose Package Pin L10 and K9.

Ok, so I look into the HW Guide (http://microzed.org/sites/default/files/documentations/MicroZed_HW_UG_v1_4.pdf) and on page 17 it tells me I reach those pins through JX1 97 and 99..

So I switch to the BKO Schematics (http://zedboard.org/sites/default/files/documentations/MBCC-BKO_RevA_Schematic_131114.pdf) to find out what pins its going to be on my breakout board. I would assume I connect my input signal to whatever pins are connected to JX1 97 and 99.

but that document says JX 97 and 99 are tied to ground? Besides I cant reach 99 from the BKO Board.

What am I missing here?

What pins on the breakout board do I have to put my input signal on?

thanks!

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello trillian,

    Yes i see on the BKO those pins are routed to GND. If you want to use those pins, may i suggest using The MicroZed IO Carrier Card?

    You can split up a differential pair into two seperate pins. It will not have any adverse affect.

    -Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 8 years ago

    Hello trillian,

    Yes i see on the BKO those pins are routed to GND. If you want to use those pins, may i suggest using The MicroZed IO Carrier Card?

    You can split up a differential pair into two seperate pins. It will not have any adverse affect.

    -Josh