Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design xapp 1079 vivado 2014.2 for microzed
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 361 subscribers
  • Views 493 views
  • Users 0 members are here
Related

xapp 1079 vivado 2014.2 for microzed

e14 Contributor
e14 Contributor over 11 years ago

Hi,
I was following Vivado Zynq SpeedWay Workshops lab 9 to create AMP application with bare-metal code on both ARM cores.

But the problem is I'm stuck at when I'm trying to make the BSP for cpu1 with error the following error:

(::sw_standalone_amp_v3_11_a::generate : invalid command name "xget_libgen_proc_handle")

I think the problem is because I'm using vivado 2014.2 and the repositories is not compatible with vivado 2014.2, and after quick search I found this www.wiki.xilinx.com/XAPP1079+Latest+Information but there are no tcl for MicroZed.

Does anyone know how to run xapp 1079 on MicroZed, or anyone happen to have dsp repositories for lab 9 for vivado 2014.2?

thanks

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    While there is not a MicroZed build included in the latest XAPP1079 there is one for the MicroZed in the latest XAPP1078 material: 

    http://www.wiki.xilinx.com/XAPP1078+Latest+Information

     

    I believe that the hardware build is the same for XAPP1078 and XAPP1079 so, while I have not tried it, you might be able to use the MicroZed files from XAPP1078 for XAPP1079.

     

    Let the forum know if you try this and are successful.

     

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 11 years ago in reply to e14 Contributor

    Thanks Gary for the reply, and yes, the repositories from xapp1078 can be used here. All it takes is to copy the avnetBoard_repo to <xapp>/design/src and copy the create_proj_microZed.tcl and create_bd_microZed.tcl from xapp1078 and change the last block of create_proj_microZed.tcl to the last block of create_proj_zedBoard.tcl from xapp1079 (the Export design to SDK part)