Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Error with Program FPGA from SDK
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 1 reply
  • Subscribers 361 subscribers
  • Views 607 views
  • Users 0 members are here
Related

Error with Program FPGA from SDK

e14 Contributor
e14 Contributor over 11 years ago

I am using a Platform Cable USB II to the JTAG connector on the Microzed.  I am able to program the fpga from Vivado successfully and get a blue light.  But if I try to do the "Program FPGA" (or when I try to Run As-> Launch on Hardware) from Xilinx SDK, I get the following message:

ERRORt: FPGA Configuration failed.Connection to Board Failed
Failed to open Cable Node jsn1 on TCP:127.0.0.1:3121

I had set the connection to "Local",so I'm not sure why it is looking at 127.0.0.1

any ideas?

  • Sign in to reply
  • Cancel

Top Replies

  • e14 Contributor
    e14 Contributor over 11 years ago +1 verified
    never mind, it's working now. not sure why, but it seemed to start working after I closed the SDK and started it up again.
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    never mind, it's working now.  not sure why, but it seemed to start working after I closed the SDK and started it up again.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Reject Answer