Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Programming MicroZed FPGA from SDK 14.7 fails
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 395 views
  • Users 0 members are here
Related

Programming MicroZed FPGA from SDK 14.7 fails

jesusmgonzalez
jesusmgonzalez over 11 years ago


Hi!

Hi followed the previous steps to get a hardware design using old tools ISE14.7 from this link:
http://zedboard.com/node/add/forum/69

I worked around this proposal, and successfully got the bitstream to export to XSDK. Then, I tried to program the FPGA of the MicroZed board with the external programmer (driver correctly installed, green led), and got this error message (at the end of programming):

"Program FPGA Failed: Failed to download the bit file"
"DONE bit didn't go HIGH after programming FPGA"

Does anybody know how to overcome this problem?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The link you provided does not work, so it is difficult to determine the issue but there are a couple of things to look at.

     

    Verify that your design targets the MicroZed board that you are using (7010 vs 7020 MicroZed).

     

    Unlike the ZedBoard the MicroZed does require an external JTAG cable for JTAG operations.

    MicroZed is designed with the Platform Cable JTAG connector, Molex 87832-1420 which is a 2.0mm 2x7 shrouded, polarized header. On MicroZed, this is J3 and is compatible with Xilinx Platform Cables and Digilent JTAG HS1 or HS2 Programming Cables.

     

    If you are using the MicroZed with one of the Carrier Cards you need to connect the external JTAG cable to the connector on the carrier card and not the MicroZed.

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    The link you provided does not work, so it is difficult to determine the issue but there are a couple of things to look at.

     

    Verify that your design targets the MicroZed board that you are using (7010 vs 7020 MicroZed).

     

    Unlike the ZedBoard the MicroZed does require an external JTAG cable for JTAG operations.

    MicroZed is designed with the Platform Cable JTAG connector, Molex 87832-1420 which is a 2.0mm 2x7 shrouded, polarized header. On MicroZed, this is J3 and is compatible with Xilinx Platform Cables and Digilent JTAG HS1 or HS2 Programming Cables.

     

    If you are using the MicroZed with one of the Carrier Cards you need to connect the external JTAG cable to the connector on the carrier card and not the MicroZed.

     

    -Gary