Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design PetaLinux SD boot
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 11 replies
  • Subscribers 362 subscribers
  • Views 3266 views
  • Users 0 members are here
Related

PetaLinux SD boot

e14 Contributor
e14 Contributor over 11 years ago

I'm having trouble figuring out how to get the image I've created for the microZed 7020 to boot on it. It runs nicely in the qemu emulator but I can't get a valid system.bit.bin file. I've found some not quiet for microZed instructions to make a .bit.bin file, but I try using any of those files the boot process ends with a timeout on DMA when trying to load the FMGA.

For reference I'm using the Avnet-MicroZed-z7020-v2014.2.bsp file with the petalinux-create command, that appears to be the most correct one to use.

SD Boot without system.bit.bin:
Copying Linux from SD to RAM...
Device: zynq_sdhci
Manufacturer ID: 2
OEM: 544d
Name: SD04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
Loading bitstream from SD/MMC/eMMC to RAM..
Device: zynq_sdhci
Manufacturer ID: 2
OEM: 544d
Name: SD04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading system.bit.bin
** Unable to read file system.bit.bin **
zynq-uboot>
]


With a system.bit.bin that I made using "bootgen -image test.bif -split bin -o i BOOT.BIN" but none of the .bit files I could find to convert with that matched the instructions so I think I'm doing something wrong there. But the boot attempts with that system.bit.bin all failed with:

Copying Linux from SD to RAM...
Device: zynq_sdhci
Manufacturer ID: 2
OEM: 544d
Name: SD04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
Loading bitstream from SD/MMC/eMMC to RAM..
Device: zynq_sdhci
Manufacturer ID: 2
OEM: 544d
Name: SD04G
Tran Speed: 50000000
Rd Block Len: 512
SD version 2.0
High Capacity: Yes
Capacity: 3.7 GiB
Bus Width: 4-bit
reading system.bit.bin
4045568 bytes read in 550 ms (7 MiB/s)
Error: Timeout waiting for DMA to complete.
fpga - loadable FPGA image support

Usage:
fpga [operation type] [device number] [image address] [image size]
fpga operations:
  dump  [dev]                   Load device to memory buffer
  info  [dev]                   list known device information
  load  [dev] [address] [size]  Load device from memory buffer
  loadb [dev] [address] [size]  Load device from bitstream buffer (Xilinx only)
  loadmk [dev] [address]        Load device generated with mkimage
        For loadmk operating on FIT format uImage address must include
        subimage unit name in the form of addr:<subimg_uname>
zynq-uboot>



Really I'm hoping someone just points me to the correct instructions for this.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Going through UG 977 they have this pearl of a line at the end of page 15:

    For Zynq, you can follow section Boot Pre-built Images from SD Card for Zynq to SD boot the rebuilt images. Instead of using the prebuilt image.ub, use the rebuilt one from <plnx-proj-root>/images/linux/image.ub

    It's just a shame that we haven't been told how to build a boot.bin file. But I bet that is only an issue because now I need to figure out how to deal with a larger image.ub.

    But if I can't solve that I'll start a new thread.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 11 years ago

    Going through UG 977 they have this pearl of a line at the end of page 15:

    For Zynq, you can follow section Boot Pre-built Images from SD Card for Zynq to SD boot the rebuilt images. Instead of using the prebuilt image.ub, use the rebuilt one from <plnx-proj-root>/images/linux/image.ub

    It's just a shame that we haven't been told how to build a boot.bin file. But I bet that is only an issue because now I need to figure out how to deal with a larger image.ub.

    But if I can't solve that I'll start a new thread.