Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design Keep Linux and custom hardware in PL at power on
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 10 replies
  • Subscribers 362 subscribers
  • Views 1245 views
  • Users 0 members are here
Related

Keep Linux and custom hardware in PL at power on

e14 Contributor
e14 Contributor over 10 years ago

MicroZED with IO Carrier. My custom hardware PL application does not need the PS at all. My TOP design does however instantiate both the Base PS_module wrapper as well as my custom PL_module. And a bit file for this TOP design can be generated in Vivado.

Powering up the MicroZED and Carrier, boots Linux from QSPI and responds to serial Terminal commands. From the Vivado GUI with JTAG connected I can "Program Device" with the TOP bit file. After programming is done both Linux and my custom hardware in the PL are operating as expected. Also as expected, when power off then on, my custom hardware in the PL is no longer operational, and the device must be programmed again.

What do I do to program this TOP bit file into the QSPI so that the system boots to the Linux and my custom hardware in the PL is running and available at power up.

Thank you

  • Sign in to reply
  • Cancel
Parents
  • jafoste4
    0 jafoste4 over 10 years ago

    Sorry Warrenh,

    I mispoke(I just corrected it above). Pulsar Linux comes pre loaded in the SD card we provide with the development kit. My guess is you were either previously running Pulsar Linux or PetaLinux as those are the two most common I see. Here is where you can find more information about them.

    PetaLinux

    http://zedboard.org/support/design/1519/10

    http://www.wiki.xilinx.com/PetaLinux

    https://www.xilinx.com/support/download/index.html/content/xilinx/en/downloadNav/embedded-design-tools/2014-4.html

    Pulsar Linux

    http://zedboard.org/support/design/1519/10

    I would also look at the Open Source Linux QSPI Image Tutorial at

    http://zedboard.org/support/design/1519/10

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jafoste4
    0 jafoste4 over 10 years ago

    Sorry Warrenh,

    I mispoke(I just corrected it above). Pulsar Linux comes pre loaded in the SD card we provide with the development kit. My guess is you were either previously running Pulsar Linux or PetaLinux as those are the two most common I see. Here is where you can find more information about them.

    PetaLinux

    http://zedboard.org/support/design/1519/10

    http://www.wiki.xilinx.com/PetaLinux

    https://www.xilinx.com/support/download/index.html/content/xilinx/en/downloadNav/embedded-design-tools/2014-4.html

    Pulsar Linux

    http://zedboard.org/support/design/1519/10

    I would also look at the Open Source Linux QSPI Image Tutorial at

    http://zedboard.org/support/design/1519/10

    --Josh

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to jafoste4

    Hello,

    Non of this reference documentation contains a u-boot.elf for the Pulsar Linux. I would desire to get  a u-boot.elf for the original Pulsar Linux to reference as the 3rd object for the Create Boot Image script for my project .mcs file. Where can I find a u-boot.elf file that would do a Second Stage Boot Load of the Pulsar Linux?

    Thank you