Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design MAC Address
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 2 replies
  • Subscribers 362 subscribers
  • Views 735 views
  • Users 0 members are here
Related

MAC Address

richw42
richw42 over 12 years ago

Is there any code in Linux or u-boot that will magically set the Ethernet MAC address if I put the right part in the right place (for example, copying the example of the carrier card), or am I responsible for writing some code?
Edit: I understand that u-boot can supply a MAC address. But I'm asking how I get an official MAC address from an attached serial eeprom into the running system. I was unable to find any code to do this, be it u-boot, kernel, a manufacture-time utility, or a utility that runs every time on boot.

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    I'm going to assume we're talking about pre-production here, because of course if a product goes out into the real world you need the device assigned a permanent unique ID from the proper authorities.

    However, there are a number of ways you can set a MAC address privately.  Check out these links:

    Changing the MAC address from Linux:
    http://en.wikibooks.org/wiki/Changing_Your_MAC_Address/Linux

    Changing the MAC address from U-boot:
    http://www.denx.de/wiki/view/DULG/UBootEnvVariables

    Generating a random MAC address for each boot:
    http://forums.xilinx.com/t5/Embedded-Linux/ZC702-get-new-MAC-address-each-time-I-boot-it/m-p/254658

    Ron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • zedhed
    0 zedhed over 12 years ago

    Hi richw42,

    This Xilinx forum thread might provide some additional insight into how MAC addressing works:

    http://forums.xilinx.com/t5/Embedded-Linux/Perm-changing-the-MAC-address/td-p/61463

    Regards,

    -Kevin