Avnet Boards Forums
  • Products & Partners
  • Dev Tools
  • Avnet & Tria Boards Community
  • Avnet Boards Forums
  • More
  • Cancel
Avnet Boards Forums
MicroZed Hardware Design axi ethernetlite
  • Forum
  • Documents
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Avnet Boards Forums to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 3 replies
  • Subscribers 361 subscribers
  • Views 750 views
  • Users 0 members are here
Related

axi ethernetlite

e14 Contributor
e14 Contributor over 12 years ago

Hello
I am trying to use the Ethernetlite IP instead of emacps,
I have disabled the emacps on  the Zynq and integrate the axi Ethernetlite IP, but this IP needs to connect the MII and MDIO to PHY  Ethernet ,
My question is how to connect MII/MDIO and is this the right way to use the Ethernet lite IP?

cheers

  • Sign in to reply
  • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    The direct connections from the Processing System (PS) of the Zynq to the MIO pins connected to the RGMII PHY on the MicroZed or the ZedBoard are not accessible from the Programmable Logic (PL). So the only way to use the EthernetLite IP in the Zynq PL would be to connect to an external PHY device via PL signal connections.

     

    One way to do this would be to connect an FMC board with a PHY, such as this board : http://www.em.avnet.com/en-us/design/drc/Pages/ISM-Networking-FMC-Module.aspx

     

    The ZedBoard has a LPC FMC connector onboard. To use this with the MicroZed you would need to use the MicroZed FMC Carrier Card: http://www.microzed.org/product/microzed-fmc-carrier

     

    -Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to e14 Contributor

    thanks Gary

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago

    Hello. Suppose that I have a FCM, is there any tutorial on how to connect the MII / MDIO ??

    Or generally how to create this specific Constraint Files??

    Thanks a lot in advance